Hello All,
I'm running the TDC7200 @ 16 MHz and have some questions about the Time1 and Time2 registers: as they are only started on the rising flank of the start and stop and related to the clock, they barely change and the maximum value is maximum one clock cycle. Is this reasoning correct?
Is a similar reasoning also valid for the calibration registers but than without taking into account the start and the stop?
Greetings.