This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, I have question about demo visualizer 3.6
my setup is : AWR 1642BOOST , mmw demo firmware SDK 3.6.
I measure distance from sensor to wall about 20 cm , and 80 cm. This is the 20 cm from demo visualizer :
X Y Scatter plot said detected object is at ( 0.017 , 0.2180134)
Range profile said detected object is at 0.1709. But if we move cursor to the peak, we will found almost similar to 0.2180
Is there something that I miss from document ?
Hello Woody,
Let me take a look at this and get back to you.
Regards,
Saswat Kumar
Hi,
Sorry for the delay.
We have seen this issue before. It is a known issue in the visualizer Range Profile Display.
The detected point information provided in the XY Scatter Plot is correct
Thank you
Cesar