Hi,
I am looking to use the TMAG5170 sensor in Active Trigger mode in order to to synchronise measurements from this sensor with other sensors in the system. I am using the ALERT line to initiate the conversion start and have the sensor pull ALERT low to indicate conversion is complete. I have this working quite nicely, however the conversion times I am seeing are much slower than those suggested by the datasheet. I instrumented my running system and produced the following table using data from logic analyser traces. The device operating mode is set to: 3h = Active trigger mode (TRIGGER_MODE active). As far as I can tell I do not have any sleep/low power modes enabled. It is also interesting to note the variation in duration for each configuration of ~64us. I presume this relates to where the alert signal falls relative to an internal clock?
I would appreciate your feedback about the below timings, are they what you would expect in this operating mode, or have I misconfigured something?
Thanks!