Hi,
I want to read the data continuously through the tmp411 sensor.
I just set temperature range bit to 1 and RES0, RES1 to 0.
But, always read "1" from the SD bit in the Configuration register.
If i read back the configuration register, read data is 0x44.(SD =1, Temperature range = 1)
Because of this, it appears that incorrect data is being read.
The actual measurement temperature is 30'C, but reading High Bytes reads 0x1E(dec 30).
I think the Temperature range bit is set to 1, so it should be read as 0x5E.
What's the problem?