Other Parts Discussed in Thread: DCA1000EVM, IWR1443
Hello,
I'm working with IWR1443BOOST+DCA1000EVM to evaluate RADAR devices.
I've run several different demos now and studied the manuals, and I find many references to power cycling the device as the way to get the SOP jumpers re-read (lines re-sensed), in case you need to change boost modes of the device during your process. (For example, in the Out of Box Demo for IWR1443, you need to change from Flashing to Functional mode). It's always specified to use NRST to force this power cycle, but I'm trying to do that in my device and it's not working.
Example:
- I connect the devices to power with SOP config 101: Flashing mode.
- I flash the binary for Out of Box Demo.
- I change the SOP jumpers to 001: Functional mode, and press NRST button (the led NRST decreases it's intensity while the button is pressed)
- I open mmWave Demo Visualizer and try to connect to my hardware. Not achieved (status: connecting)
So no actual power cycle is being carried out. Nevertheless, when I manually power cycle the device (unplug and plug the supply jag), I manage to connect with mmWave.
This is happening in every context I need to change SOP values (I need to do a manual reset because NRST button is not actually doing nothing).
What could be happening?
- Am I not understanding NRST button function?
- It's my device NRST button not functioning?
- Is there an aditional step to power cycle the device and sense the SOP lines that I'm missing?
Thanks in advance,
Julia Sanchez.