This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: Can I use the IWR6843AOP with a MMWAVEICBOOST Launch Pad SPI connections

Part Number: IWR6843AOP
Other Parts Discussed in Thread: MMWAVEICBOOST

I've updated an example lab (3d people counting) to send data to the SPI bus. The Bus opens fine and and the spi transfer command is called (with no erro), however it never returns and is stuck in an infinite loop  due to  MIBSPI_checkTGComplete status 1 is never returned. I've set the DPI switches on the AOP board as per documentation. I'm at a loss as to what i may have missed. We're using a raspberry pi as our spi master and it all checks outs. 

Any help would go a long way