Hi,
I'm using out-of-box demo of mmwave_sdk_03_06_00_00 in IWR1843.
Assume I have two sensors woking in 80-81G and 77-79G with the same slope respectively. It seems the interference doesn't happen according to my experiments. I think there should be some filter which checks the IF freqency <= 1G.
There is a customer requirment about using the 77-79G sensor to detect the 80-81G sensor based on interference, I think it can be achieved by turn off the IF frequency checking.
Hence, where are codes related to the IF frequency checking?
Thanks.