Other Parts Discussed in Thread: IWR6843ISK, UNIFLASH
Hello everyone,
I am currently trying to acquire sensor raw data with a DCA1000EVM and an IWR6843ISK EVM. I did this prior. but at the moment it is not working. I have switched to a new PC and am at a loss what to do.
All configuration runs without error, but when i press DCA1000ARM and try to trigger a frame, i get a Response timeout. Does anyone see an obvious problem?
[09:23:53] [RadarAPI]: ar1.selectRadarMode(0) [09:23:54] [RadarAPI]: Status: Passed [09:23:54] Matlab Runtime Engine is installed [09:23:54] [RadarAPI]: Starting Matlab Engine.. [09:24:11] [RadarAPI]: Matlab Engine Started! [09:24:14] [RadarAPI]: ar1.selectCascadeMode(0) [09:24:14] [RadarAPI]: Status: Passed [09:24:14] [RadarAPI]: ar1.LoadSettings('C:\Users\stoer\AppData\Roaming\RSTD\ar1gui.ini') [09:24:14] [RadarAPI]: Error: Index was outside the bounds of the array. [09:24:14] Trace: [09:24:14] at AR1xController.ScriptOps.getMatlabPostProcVersion() [09:24:14] TESTING = false [09:24:14] RstdNet: Port 2777: Listening.. [09:24:14] [09:24:14] ***Script completed successfully.*** [09:29:04] [RadarAPI]: Opening Gpio Control Port() [09:29:04] [RadarAPI]: Status: Passed [09:29:05] [RadarAPI]: Opening Board Control Port() [09:29:05] [RadarAPI]: Status: Passed [09:29:06] [RadarAPI]: ar1.FullReset() [09:29:06] [RadarAPI]: Status: Passed [09:29:06] [RadarAPI]: Closing Board Control Port() [09:29:06] [RadarAPI]: Status: Passed [09:29:07] [RadarAPI]: Closing Gpio Control Port() [09:29:07] [RadarAPI]: Status: Passed [09:29:07] [RadarAPI]: ar1.SOPControl(2) [09:29:07] [RadarAPI]: Status: Passed [09:29:07] [RadarAPI]: ar1.Connect(3,115200,1000) [09:29:08] [RadarAPI]: ar1.Calling_IsConnected() [09:29:10] [RadarAPI]: ar1.SelectChipVersion("IWR6843") [09:29:10] [RadarAPI]: Status: Passed [09:29:10] [RadarAPI]: ar1.frequencyBandSelection("60G") [09:29:10] [RadarAPI]: ar1.SelectChipVersion("IWR6843") [09:29:10] [RadarAPI]: Status: Passed [09:29:10] Device Status : IWR6843/QM/SOP:2/ES:2 [09:29:10] [RadarAPI]: ar1.SaveSettings('C:\Users\stoer\AppData\Roaming\RSTD\ar1gui.ini') [09:29:11] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\radarss\\xwr68xx_radarss.bin") [09:29:11] [RadarAPI]: Downloading BSS ROM RPRC Binary.. [09:29:56] [RadarAPI]: ar1.GetBSSFwVersion() [09:29:56] [RadarAPI]: BSSFwVersion:(06.02.00.06 (22/08/19)) [09:30:50] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\masterss\\xwr68xx_masterss.bin") [09:30:51] [RadarAPI]: Downloading MSS RPRC Binary.. [09:31:09] [RadarAPI]: ar1.GetMSSFwVersion() [09:31:09] [RadarAPI]: MSSFwVersion:(02.00.00.03 (27/08/19)) [09:33:32] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0) [09:33:32] [RadarAPI]: Status: Passed [09:33:32] MSS power up done async event received! [09:33:34] [RadarAPI]: ar1.SelectChipVersion("IWR6843") [09:33:34] [RadarAPI]: Status: Passed [09:33:34] [RadarAPI]: ar1.SelectChipVersion("IWR6843") [09:33:34] [RadarAPI]: Status: Passed [09:33:34] Device Status : IWR6843/QM/SOP:2/ES:2 [09:33:34] [RadarAPI]: ar1.RfEnable() [09:33:34] BSS power up done async event received! [09:33:34] [RadarAPI]: Status: Passed [09:33:34] [RadarAPI]: ar1.GetMSSFwVersion() [09:33:34] [RadarAPI]: MSSFwVersion:(02.00.00.03 (27/08/19)) [09:33:35] [RadarAPI]: ar1.GetBSSFwVersion() [09:33:35] [RadarAPI]: BSSFwVersion:(06.02.00.06 (22/08/19)) [09:33:38] [RadarAPI]: ar1.GetCaptureCardDllVersion() [09:33:38] [RadarAPI]: Sending dll_version command to DCA1000 [09:33:38] [RadarAPI]: [09:33:38] DLL Version : 1.0 [09:33:38] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000") [09:33:38] [RadarAPI]: Status: Passed [09:33:39] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098) [09:33:39] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30) [09:33:39] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25) [09:33:39] [RadarAPI]: Sending fpga command to DCA1000 [09:33:39] [RadarAPI]: [09:33:39] FPGA Configuration command : Success [09:33:39] [RadarAPI]: Sending record command to DCA1000 [09:33:40] [RadarAPI]: [09:33:40] Configure Record command : Success [09:33:40] [RadarAPI]: ar1.GetCaptureCardFPGAVersion() [09:33:40] [RadarAPI]: Sending fpga_version command to DCA1000 [09:33:40] [RadarAPI]: [09:33:40] [09:33:40] FPGA Version : 2.8 [Record] [09:33:40] [09:33:57] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 1, 1, 1, 1, 1, 2, 1, 131072) [09:33:57] [RadarAPI]: Status: Passed [09:33:58] [RadarAPI]: ar1.LPModConfig(0, 0) [09:33:58] [RadarAPI]: Status: Passed [09:33:59] [RadarAPI]: ar1.RfInit() [09:33:59] RF Init async event received! [09:33:59] [RadarAPI]: Status: Passed [09:33:59] [RadarAPI]: Time stamp, Temperture: 25225,41; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 0, 0; HPFcutoff Status, Update: 0, 0; LPFcutoff Status, Update: 0, 0; PeakDetector Status, Update: 0, 0; TxPower Status, Update: 0, 0; RxGain Status, Update: 0, 0; TxPhase Status, Update: 0, 0; RxIQMM Status, Update: 0, 0; [09:34:04] [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0) [09:34:04] [RadarAPI]: Status: Passed [09:34:06] [RadarAPI]: ar1.LvdsClkConfig(1, 1) [09:34:06] [RadarAPI]: Status: Passed [09:34:07] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0) [09:34:07] [RadarAPI]: Status: Passed [09:34:14] [RadarAPI]: ar1.ProfileConfig(0, 60, 7, 5, 56,9, 0, 0, 0, 0, 0, 0, 70,283, 0, 256, 5000, 0, 0, 48) [09:34:14] [RadarAPI]: Status: Passed [09:34:22] [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0) [09:34:22] [RadarAPI]: Status: Passed [09:34:22] [RadarAPI]: ar1.ChirpConfig(1, 1, 0, 0, 0, 0, 0, 0, 1, 0) [09:34:22] [RadarAPI]: Status: Passed [09:34:22] [RadarAPI]: ar1.ChirpConfig(2, 2, 0, 0, 0, 0, 0, 0, 0, 1) [09:34:22] [RadarAPI]: Status: Passed [09:34:36] Test Source Already Disabled...!!! [09:34:36] [RadarAPI]: ar1.DisableTestSource(0) [09:34:36] [RadarAPI]: Status: Passed [09:34:36] [RadarAPI]: ar1.FrameConfig(0, 0, 16, 1, 100, 0, 0, 1) [09:34:36] [RadarAPI]: Status: Passed [09:34:42] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1) [09:34:42] [RadarAPI]: Sending start_record command to DCA1000 [09:34:44] [RadarAPI]: ar1.StartFrame() [09:34:48] Status: Failed, Error Type: RESP TIMEOUT [09:35:12] [RadarAPI]: [09:35:12] Start Record command : Success [09:35:12] [09:35:12] No LVDS data [09:35:12] [09:35:12] Record stop is done successfully [09:40:47] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1) [09:40:47] [RadarAPI]: Sending start_record command to DCA1000 [09:40:48] [RadarAPI]: ar1.StartFrame() [09:40:52] Status: Failed, Error Type: RESP TIMEOUT [09:41:17] [RadarAPI]: [09:41:17] Start Record command : Success [09:41:17] [09:41:17] No LVDS data [09:41:17] [09:41:17] Record stop is done successfully