Other Parts Discussed in Thread: TMP411
Hi TI expert,
Few questions would like to check with you.
1. The Table shows that different version of TMP411-Q1 has different default Local/Remote temp limit.
I notice we can change "Configuration Register" bit 2 to "1" to extend the range.
Does it means once we change the bit 2, we can measure the temp from -40oC~85oC even we use the TMP411/A/B/C-Q1 version?
2. The datasheet mentioned that the 21oC in extended temp mode but I'm not sure what does that mean.
And the 21oC does not match the description in the Table 6.
3. Since the ABS max rating table shows the operating temp range is able to support from -55oC ~ 127oc so I believe the TMP411A/B/C/D version can measure the temp range within it, am I right?
Looking forward to your reply.
Thank you.