What is the tolerance of the output voltages for respective temperatures?, In data sheet the given is fixed voltage value.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the tolerance of the output voltages for respective temperatures?, In data sheet the given is fixed voltage value.
Hi Ravi,
The tolerances you are looking for would be specified in the device accuracy spec. The temperature coefficient for the TMP235-Q1 is 10 mV/°C. I've included a document in attachment that provides the look up table with voltages for min and max voltage values as well.
Jalen