Hi Team,
The DRV5013 datasheet describe the VCC power should have less than 50mVpp variation. The reuqirement looks strict, especially in high VCC application, for example:
For 3.3V power supply, 0.05V/3.3V*100%=1.5%,
For 18V power supply, 0.05V/18V*100%=0.27%
It is really tough to get such high accuracy power, and when used in BLDC, the power will change significant during motor start-up, if we use 18V to power DRV5013 directly, it is impossible to meet 50mV requirement.
May I have your DRV5013 power supply recommendation for 18V rail? thanks.