Other Parts Discussed in Thread: TDC1000, TIDA-00322, TDC1000-C2000EVM, TUSS4470, UCC27531-Q1
I study TIDA-00322evm introduction and circuit design , it is introduced with 1MHz sensor and 30V high voltage added.
If we have ultrasonic sensor( the frequency is 2 MHz) to test the water level and would adopt TIDA-00322 suggested circuit design to get good performance, which components need to be changed ? which circuit needs to be modified expect the Tx frequency changed to 2MHz ?
Ex: external bandpass filter ? high voltage driving circuit ? ….. etc ??
Is there opportunity to test the water level up to 1.5 meter ? thanks ~