Accoring to datasheet, setting EN_TEMP_CORR to 1 enables the illumination crosstalk temperature calibration.
But there is two kind of illumination crosstalk temperature calibration, one using internal temp sensor and another one using external temp sensor which has higher resolution.
How do it specify the type of illumination crosstalk calibration to enable?
I can't kind it in datasheet.