Other Parts Discussed in Thread: AWR2243
I am using the "PROCESSOR_SDK_CASCADE_RADAR_03_08_00_00_prebuilt.exe" which is downloaded from :
https://software-dl.ti.com/processor-sdk-vision/esd/TDAx/vision-sdk/latest/index_FDS.html
After installation on Windows, it includes the "sdimage.img.xz" for windows, and "prebuild_linux.zip" for linux.
The sdimage.img.xz works well. When flash it into the SD card, the eth0 interface obtains an IP address via DHCP, and ping other hosts successfully.
The "prebuild_linux.zip" includes 4 files : MLO, u-boot.img, uenv.txt, tisdk-rootfs-image-dra7xx-evm.tar.xz.
When flash it into the SD card following the section 4.2 of "VisionSDK_Linux_UserGuide.pdf" in Vision SDK v03.08, the DSP-EVM board cannot obtain IP address via DHCP on the eth0 interface, and cannot ping any host when adding a static ip address to the eth0 interface.
Please find the log file from the DSP board when it is boot from SD.
U-Boot 2019.01-00016-gd32beeb (Dec 26 2019 - 17:36:13 +0530) CPU : DRA752-GP ES2.0 Model: TI DRA742 Board: DRA74x Cascade EVM REV H.4 DRAM: 4 GiB NAND: 0 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Loading Environment from MMC... Card did not respond to voltage select! *** Warning - No block device, using default environment Card did not respond to voltage select! invalid mmc device Net: Warning: ethernet@48484000 using MAC address from ROM eth0: ethernet@48484000 Hit any key to stop autoboot: 0 i2c_write: error waiting for data ACK (status=0x116) pcf8575_i2c_write_le16 i2c write failed to addr 21 switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 ** Unable to read file boot.scr ** 185 bytes read in 1 ms (180.7 KiB/s) Loaded env from uEnv.txt Importing environment from mmc0 ... switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 4411904 bytes read in 193 ms (21.8 MiB/s) 97317 bytes read in 6 ms (15.5 MiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8ffe5000, end 8ffffc24 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.19.73-00041-gf456dbc (x0284921@bangvideoapps02) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 SMP PREEMPT Thu Dec 26 17:37:33 IST 2019 [ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d [ 0.000000] CPU: div instructions available: patching division code [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache [ 0.000000] OF: fdt: Machine model: TI DRA742 Cascade Radar Board [ 0.000000] Memory policy: Data cache writealloc [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created DMA memory pool at 0x0000000040300000, size 3 MiB [ 0.000000] OF: reserved mem: initialized node cmem@40300000, compatible id shared-dma-pool [ 0.000000] Reserved memory: regions without no-map are not yet supported [ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 80 MiB [ 0.000000] OF: reserved mem: initialized node ipu2-memory@95800000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created CMA memory pool at 0x000000009e000000, size 32 MiB [ 0.000000] OF: reserved mem: initialized node ipu1-memory@9d000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: regions without no-map are not yet supported [ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a1000000, size 32 MiB [ 0.000000] OF: reserved mem: initialized node dsp1-memory@99000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a3000000, size 32 MiB [ 0.000000] OF: reserved mem: initialized node dsp2-memory@9f000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: regions without no-map are not yet supported [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 64 MiB [ 0.000000] OF: reserved mem: initialized node cmem@A9000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created CMA memory pool at 0x00000000b0000000, size 64 MiB [ 0.000000] OF: reserved mem: initialized node gpu-memory@c0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: regions without no-map are not yet supported [ 0.000000] cma: Reserved 64 MiB at 0x00000000bc000000 [ 0.000000] OMAP4: Map 0x000000027fd00000 to (ptrval) for dram barrier [ 0.000000] DRA752 ES2.0 [ 0.000000] random: get_random_bytes called from start_kernel+0xb4/0x470 with crng_init=0 [ 0.000000] percpu: Embedded 16 pages/cpu s36492 r8192 d20852 u65536 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1025330 [ 0.000000] Kernel command line: console=ttyO0,115200n8 vram=16M root=PARTUUID=2eec288c-02 rw rootwait ip=none cma=64M vmalloc=128M [ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes) [ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Memory: 2366896K/4109312K available (10240K kernel code, 341K rwdata, 2804K rodata, 2048K init, 269K bss, 1431120K reserved, 311296K cma-reserved, 2167808K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xf8000000 - 0xff800000 ( 120 MB) [ 0.000000] lowmem : 0xc0000000 - 0xf7800000 ( 888 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (12256 kB) [ 0.000000] .init : 0x(ptrval) - 0x(ptrval) (2048 kB) [ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 342 kB) [ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) ( 270 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] Tasks RCU enabled. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] GIC: Using split EOI/Deactivate mode [ 0.000000] OMAP clockevent source: timer1 at 32786 Hz [ 0.000000] arch_timer: cp15 timer(s) running at 6.14MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns [ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns [ 0.000018] Switching to timer-based delay loop, resolution 162ns [ 0.000296] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns [ 0.000305] OMAP clocksource: 32k_counter at 32768 Hz [ 0.000775] Console: colour dummy device 80x30 [ 0.000795] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0' [ 0.000803] This ensures that you still see kernel messages. Please [ 0.000811] update your kernel commandline. [ 0.000845] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475) [ 0.000863] pid_max: default: 32768 minimum: 301 [ 0.000984] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000999] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.001547] CPU: Testing write buffer coherency: ok [ 0.001582] CPU0: Spectre v2: using ICIALLU workaround [ 0.001797] /cpus/cpu@0 missing clock-frequency property [ 0.001817] /cpus/cpu@1 missing clock-frequency property [ 0.001830] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 [ 0.059918] Setting up static identity map for 0x80200000 - 0x80200060 [ 0.079930] rcu: Hierarchical SRCU implementation. [ 0.100120] EFI services will not be available. [ 0.119990] smp: Bringing up secondary CPUs ... [ 0.200345] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001 [ 0.200351] CPU1: Spectre v2: using ICIALLU workaround [ 0.200474] smp: Brought up 1 node, 2 CPUs [ 0.200486] SMP: Total of 2 processors activated (24.59 BogoMIPS). [ 0.200495] CPU: All CPU(s) started in HYP mode. [ 0.200503] CPU: Virtualization extensions available. [ 0.201058] devtmpfs: initialized [ 0.218832] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0 [ 0.219092] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.219112] futex hash table entries: 512 (order: 3, 32768 bytes) [ 0.223936] pinctrl core: initialized pinctrl subsystem [ 0.224457] DMI not present or invalid. [ 0.224736] NET: Registered protocol family 16 [ 0.225930] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.226870] omap_hwmod: l3_main_2 using broken dt data from ocp [ 0.419976] cpuidle: using governor ladder [ 0.420013] cpuidle: using governor menu [ 0.430063] OMAP GPIO hardware version 0.1 [ 0.452840] No ATAGs? [ 0.452917] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers. [ 0.452932] hw-breakpoint: maximum watchpoint size is 8 bytes. [ 0.453453] omap4_sram_init:Unable to allocate sram needed to handle errata I688 [ 0.453466] omap4_sram_init:Unable to get sram pool needed to handle errata I688 [ 0.454093] OMAP DMA hardware revision 0.0 [ 0.465614] edma 43300000.edma: memcpy is disabled [ 0.469000] edma 43300000.edma: TI EDMA DMA engine driver [ 0.476064] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported) [ 0.477751] evm_3v3: supplied by evm_12v0 [ 0.478055] evm_5v0: supplied by evm_12v0 [ 0.478346] evm_3v6: supplied by evm_5v0 [ 0.481134] omap-iommu 40d01000.mmu: 40d01000.mmu registered [ 0.481316] omap-iommu 40d02000.mmu: 40d02000.mmu registered [ 0.481555] omap-iommu 58882000.mmu: 58882000.mmu registered [ 0.481794] omap-iommu 55082000.mmu: 55082000.mmu registered [ 0.482164] omap-iommu 41501000.mmu: 41501000.mmu registered [ 0.482336] omap-iommu 41502000.mmu: 41502000.mmu registered [ 0.482612] iommu: Adding device 55020000.ipu to group 2 [ 0.482736] iommu: Adding device 40800000.dsp to group 0 [ 0.482959] iommu: Adding device 41000000.dsp to group 3 [ 0.484118] SCSI subsystem initialized [ 0.485358] palmas 0-0058: IRQ missing: skipping irq request [ 0.510948] palmas 0-0058: Muxing GPIO 2e, PWM 0, LED 0 [ 0.512624] SMPS123: supplied by regulator-dummy [ 0.514489] SMPS45: supplied by regulator-dummy [ 0.516330] SMPS6: supplied by regulator-dummy [ 0.518028] SMPS7: supplied by regulator-dummy [ 0.518399] smps7: Bringing 1190000uV into 1150000-1150000uV [ 0.520651] SMPS8: supplied by regulator-dummy [ 0.522351] SMPS9: supplied by regulator-dummy [ 0.523320] LDO1: supplied by regulator-dummy [ 0.531422] LDO2: supplied by regulator-dummy [ 0.541285] LDO3: supplied by regulator-dummy [ 0.541629] random: fast init done [ 0.551294] LDO4: supplied by regulator-dummy [ 0.551996] LDO5: supplied by regulator-dummy [ 0.552701] LDO6: supplied by regulator-dummy [ 0.553403] LDO7: supplied by regulator-dummy [ 0.554111] LDO8: supplied by regulator-dummy [ 0.554810] LDO9: supplied by regulator-dummy [ 0.561338] LDOLN: supplied by regulator-dummy [ 0.571355] LDOUSB: supplied by regulator-dummy [ 0.583499] pcf857x: probe of 0-0020 failed with error -121 [ 0.583753] pcf857x: probe of 0-0021 failed with error -121 [ 0.584074] pca953x 0-0076: 0-0076 supply vcc not found, using dummy regulator [ 0.584134] pca953x 0-0076: Linked as a consumer to regulator.0 [ 0.584886] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz [ 0.585339] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz [ 0.585555] media: Linux media interface: v0.10 [ 0.585594] videodev: Linux video capture interface: v2.00 [ 0.585674] pps_core: LinuxPPS API ver. 1 registered [ 0.585684] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.585704] PTP clock support registered [ 0.585734] EDAC MC: Ver: 3.0.0 [ 0.586507] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400 [ 0.586753] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400 [ 0.587252] Advanced Linux Sound Architecture Driver Initialized. [ 0.588049] clocksource: Switched to clocksource arch_sys_counter [ 0.596033] NET: Registered protocol family 2 [ 0.596617] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes) [ 0.596646] TCP established hash table entries: 8192 (order: 3, 32768 bytes) [ 0.596709] TCP bind hash table entries: 8192 (order: 4, 65536 bytes) [ 0.596835] TCP: Hash tables configured (established 8192 bind 8192) [ 0.596906] UDP hash table entries: 512 (order: 2, 16384 bytes) [ 0.596940] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes) [ 0.597067] NET: Registered protocol family 1 [ 0.617509] RPC: Registered named UNIX socket transport module. [ 0.617521] RPC: Registered udp transport module. [ 0.617529] RPC: Registered tcp transport module. [ 0.617537] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.618607] hw perfevents: no interrupt-affinity property for /pmu, guessing. [ 0.618814] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available [ 0.619789] Initialise system trusted keyrings [ 0.619917] workingset: timestamp_bits=14 max_order=20 bucket_order=6 [ 0.624886] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.635374] NFS: Registering the id_resolver key type [ 0.635398] Key type id_resolver registered [ 0.635407] Key type id_legacy registered [ 0.635445] ntfs: driver 2.1.32 [Flags: R/O]. [ 0.637024] Key type asymmetric registered [ 0.637035] Asymmetric key parser 'x509' registered [ 0.637083] bounce: pool size: 64 pages [ 0.637120] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.637132] io scheduler noop registered [ 0.637141] io scheduler deadline registered [ 0.637236] io scheduler cfq registered (default) [ 0.637246] io scheduler mq-deadline registered [ 0.637255] io scheduler kyber registered [ 0.643498] pinctrl-single 4a003400.pinmux: 282 pins, size 1128 [ 0.647384] dra7-pcie 51000000.pcie: Linked as a consumer to phy-4a094000.pciephy.1 [ 0.647415] dra7-pcie 51000000.pcie: Linked as a consumer to phy-4a095000.pciephy.2 [ 0.648106] dra7-pcie 51000000.pcie: WA for Errata i870 not applied [ 0.648200] dra7-pcie 51000000.pcie: host bridge /ocp/axi@0/pcie@51000000 ranges: [ 0.648243] dra7-pcie 51000000.pcie: IO 0x20003000..0x20012fff -> 0x00000000 [ 0.648270] dra7-pcie 51000000.pcie: MEM 0x20013000..0x2fffffff -> 0x20013000 [ 0.748368] dra7-pcie 51000000.pcie: Link up [ 0.748499] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00 [ 0.748514] pci_bus 0000:00: root bus resource [bus 00-ff] [ 0.748525] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] [ 0.748537] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff] [ 0.754635] PCI: bus0: Fast back to back transfers disabled [ 0.755586] pci 0000:01:00.0: 8.000 Gb/s available PCIe bandwidth, limited by 5 GT/s x2 link at 0000:00:00.0 (capable of 63.012 Gb/s with 16 GT/s x4 link) [ 0.783638] PCI: bus1: Fast back to back transfers disabled [ 0.783682] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff 64bit] [ 0.783703] pci 0000:00:00.0: BAR 8: assigned [mem 0x20200000-0x202fffff] [ 0.783720] pci 0000:01:00.0: BAR 0: assigned [mem 0x20200000-0x20203fff 64bit] [ 0.783771] pci 0000:00:00.0: PCI bridge to [bus 01-ff] [ 0.783785] pci 0000:00:00.0: bridge window [mem 0x20200000-0x202fffff] [ 0.784091] pcieport 0000:00:00.0: Signaling PME with IRQ 168 [ 0.784247] pcieport 0000:00:00.0: AER enabled with IRQ 168 [ 0.784357] dra7-pcie 51000000.pcie: CFG 'Memory Space Enable' change [ 0.788394] evm_1v8: supplied by smps9 [ 0.788648] evm_3v3_sw: supplied by sysen1 [ 0.788883] aic_dvdd: supplied by evm_3v3_sw [ 0.832528] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.836073] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 42, base_baud = 3000000) is a 8250 [ 2.106275] console [ttyS0] enabled [ 2.110698] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 43, base_baud = 3000000) is a 8250 [ 2.120347] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 44, base_baud = 3000000) is a 8250 [ 2.131404] omap_rng 48090000.rng: Random Number Generator ver. 20 [ 2.131723] random: crng init done [ 2.138674] omapdss_dss 58000000.dss: Linked as a consumer to regulator.24 [ 2.148089] DSS: OMAP DSS rev 6.1 [ 2.153047] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops) [ 2.173207] brd: module loaded [ 2.182448] loop: module loaded [ 2.186285] vmemexp device MAJOR num = 244 [ 2.190444] vmemexp class registered [ 2.194138] /dev/vmemexp device registered [ 2.198275] ioctl DBUFIOC_EXPORT_VIRTMEM = -1072899120 [ 2.214594] nvme nvme0: pci function 0000:01:00.0 [ 2.219387] nvme 0000:01:00.0: enabling device (0140 -> 0142) [ 2.223375] m25p80 spi0.0: found n25q00, expected s25fl256s1 [ 2.231159] m25p80 spi0.0: n25q00 (131072 Kbytes) [ 2.236013] 10 fixed-partitions partitions found on MTD device spi0.0 [ 2.242504] Creating 10 MTD partitions on "spi0.0": [ 2.247409] 0x000000000000-0x000000010000 : "QSPI.SPL" [ 2.253288] 0x000000010000-0x000000020000 : "QSPI.SPL.backup1" [ 2.259832] 0x000000020000-0x000000030000 : "QSPI.SPL.backup2" [ 2.266348] 0x000000030000-0x000000040000 : "QSPI.SPL.backup3" [ 2.272888] 0x000000040000-0x000000140000 : "QSPI.u-boot" [ 2.278986] 0x000000140000-0x0000001c0000 : "QSPI.u-boot-spl-os" [ 2.285660] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env" [ 2.292105] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1" [ 2.299243] 0x0000001e0000-0x0000009e0000 : "QSPI.kernel" [ 2.305331] 0x0000009e0000-0x000002000000 : "QSPI.file-system" [ 2.312439] libphy: Fixed MDIO Bus: probed [ 2.338741] nvme nvme0: Shutdown timeout set to 10 seconds [ 2.347430] nvme0n1: p1 [ 2.378073] davinci_mdio 48485000.mdio: davinci mdio revision 1.6, bus freq 1000000 [ 2.385770] libphy: 48485000.mdio: probed [ 2.392793] mdio_bus 48485000.mdio: MDIO device at address 3 is missing. [ 2.399555] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver TI DP83867 [ 2.408644] cpsw 48484000.ethernet: Detected MACID = 94:a9:a8:bf:1a:7c [ 2.415245] cpsw 48484000.ethernet: initialized cpsw ale version 1.4 [ 2.421653] cpsw 48484000.ethernet: ALE Table size 1024 [ 2.426941] cpsw 48484000.ethernet: cpts: overflow check period 500 (jiffies) [ 2.434957] cpsw 48484000.ethernet: cpsw: Detected MACID = 94:a9:a8:bf:1a:7d [ 2.443622] i2c /dev entries driver [ 2.452193] cpu cpu0: Linked as a consumer to regulator.9 [ 2.457693] cpu cpu0: Linked as a consumer to regulator.31 [ 2.464579] sdhci: Secure Digital Host Controller Interface driver [ 2.470804] sdhci: Copyright(c) Pierre Ossman [ 2.476093] sdhci-pltfm: SDHCI platform and OF driver helper [ 2.483006] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22) [ 2.492035] sdhci-omap 4809c000.mmc: Got CD GPIO [ 2.496855] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.30 [ 2.503969] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.15 [ 2.510887] sdhci-omap 4809c000.mmc: Dropping the link to regulator.15 [ 2.517521] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.3 [ 2.524523] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.15 [ 2.531533] sdhci-omap 4809c000.mmc: no pinctrl state for ddr_1_8v mode [ 2.538208] sdhci-omap 4809c000.mmc: no pinctrl state for ddr_3_3v mode [ 2.544855] sdhci-omap 4809c000.mmc: no pinctrl state for hs200_1_8v mode [ 2.578281] mmc0: SDHCI controller on 4809c000.mmc [4809c000.mmc] using ADMA [ 2.586274] sdhci-omap 480b4000.mmc: Linked as a consumer to regulator.2 [ 2.593120] sdhci-omap 480b4000.mmc: Dropping the link to regulator.2 [ 2.599796] sdhci-omap 480b4000.mmc: Linked as a consumer to regulator.2 [ 2.630878] mmc1: SDHCI controller on 480b4000.mmc [480b4000.mmc] using ADMA [ 2.639081] ledtrig-cpu: registered to indicate activity on CPUs [ 2.650137] tlv320aic3x-codec 0-0019: Linked as a consumer to regulator.4 [ 2.657114] tlv320aic3x-codec 0-0019: Linked as a consumer to regulator.5 [ 2.665421] davinci-mcasp 4847c000.mcasp: invalid tdm slots: 0 [ 2.673020] NET: Registered protocol family 10 [ 2.678533] Segment Routing with IPv6 [ 2.682321] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 2.688360] mmc0: host does not support reading read-only switch, assuming write-enable [ 2.696968] NET: Registered protocol family 17 [ 2.701664] Key type dns_resolver registered [ 2.706086] Registering SWP/SWPB emulation handler [ 2.710977] omap_voltage_late_init: Voltage driver support not added [ 2.717562] Power Management for TI OMAP4+ devices. [ 2.723586] Loading compiled-in X.509 certificates [ 2.740749] ti-iodelay 4844a000.padconf: Set reg 0x618 Delay(a: 1076 g: 330), Elements(C=2 F=15)0x2904f [ 2.750272] ti-iodelay 4844a000.padconf: Set reg 0x620 Delay(a: 1271 g: 0), Elements(C=3 F=3)0x29063 [ 2.759571] ti-iodelay 4844a000.padconf: Set reg 0x624 Delay(a: 722 g: 0), Elements(C=1 F=11)0x2902b [ 2.768855] ti-iodelay 4844a000.padconf: Set reg 0x628 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000 [ 2.768879] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 2.777810] ti-iodelay 4844a000.padconf: Set reg 0x62c Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000 [ 2.784463] [drm] No driver support for vblank timestamp query. [ 2.793534] ti-iodelay 4844a000.padconf: Set reg 0x630 Delay(a: 751 g: 0), Elements(C=1 F=12)0x2902c [ 2.808773] ti-iodelay 4844a000.padconf: Set reg 0x634 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000 [ 2.808900] [drm] Initialized vdrm 1.0.0 20191105 for 44000000.ocp:vdrm@0 on minor 0 [ 2.817721] ti-iodelay 4844a000.padconf: Set reg 0x638 Delay(a: 20 g: 0), Elements(C=0 F=0)0x29000 [ 2.834556] ti-iodelay 4844a000.padconf: Set reg 0x63c Delay(a: 256 g: 0), Elements(C=0 F=9)0x29009 [ 2.843702] ti-iodelay 4844a000.padconf: Set reg 0x640 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000 [ 2.852662] ti-iodelay 4844a000.padconf: Set reg 0x644 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000 [ 2.861764] ti-iodelay 4844a000.padconf: Set reg 0x648 Delay(a: 263 g: 0), Elements(C=0 F=9)0x29009 [ 2.871009] ti-iodelay 4844a000.padconf: Set reg 0x64c Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000 [ 2.880088] ti-iodelay 4844a000.padconf: Set reg 0x650 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000 [ 2.889168] ti-iodelay 4844a000.padconf: Set reg 0x654 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000 [ 2.898254] ti-iodelay 4844a000.padconf: Set reg 0x658 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000 [ 2.907322] ti-iodelay 4844a000.padconf: Set reg 0x65c Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000 [ 2.916429] mmc0: new ultra high speed DDR50 SDHC card at address e624 [ 2.929146] mmcblk0: mmc0:e624 SS08G 7.40 GiB [ 2.946795] mmcblk0: p1 p2 [ 2.998616] Console: switching to colour frame buffer device 240x67 [ 3.024373] vdrm 44000000.ocp:vdrm@0: fb0: DRM emulated frame buffer device [ 3.031974] dmm 4e000000.dmm: workaround for errata i878 in use [ 3.039640] dmm 4e000000.dmm: initialized all PAT entries [ 3.045911] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 1 [ 3.056369] hctosys: unable to open rtc device (rtc0) [ 3.062238] aic_dvdd: disabling [ 3.065582] ldousb: disabling [ 3.068901] ALSA device list: [ 3.071882] No soundcards found. [ 3.205043] EXT4-fs (mmcblk0p2): recovery complete [ 3.210522] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 3.218702] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 3.229129] devtmpfs: mounted [ 3.233419] Freeing unused kernel memory: 2048K [ 3.238140] Run /sbin/init as init process [ 3.398067] systemd[1]: System time before build time, advancing clock. [ 3.415984] systemd[1]: systemd 239 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 3.437802] systemd[1]: Detected architecture arm. Welcome to Arago 2019.09! [ 3.480836] systemd[1]: Set hostname to <dra7xx-evm>. [ 3.607575] systemd[1]: File /lib/systemd/system/systemd-journald.service:36 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling. [ 3.624777] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.) [ 3.719698] systemd[1]: Configuration file /lib/systemd/system/systemd-vsdk.service is marked executable. Please remove executable permission bits. Proceeding anyway. [ 3.736909] systemd[1]: /lib/systemd/system/systemd-vsdk.service:3: Failed to add dependency on rc.pvr, ignoring: Invalid argument [ 3.854392] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 3.888579] systemd[1]: Listening on udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 3.918159] systemd[1]: Reached target Slices. [ OK ] Reached target Slices. [ OK ] Listening on udev Control Socket. [ OK ] Reached target Swap. [ OK ] Listening on Network Service Netlink Socket. [ OK ] Listening on Journal Socket (/dev/log). [ OK ] Reached target Remote File Systems. [ OK ] Created slice system-getty.slice. [ OK ] Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Forward Password Requests to Wall Directory Watch. [ OK ] Reached target Paths. [ OK ] Listening on Process Core Dump Socket. [ OK ] Listening on initctl Compatibility Named Pipe. [ OK ] Listening on Journal Socket. Starting Journal Service... Mounting POSIX Message Queue File System... Starting udev Coldplug all Devices... Mounting Kernel Debug File System... Mounting Temporary Directory (/tmp)... Starting Load Kernel Modules... Starting Remount Root and Kernel File Systems... [ OK ] Created slice system-serial\x2dgetty.slice. [ 4.563236] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) [ OK ] Started Journal Service. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Kernel Debug File System. [ OK ] Mounted Temporary Directory (/tmp). [FAILED] Failed to start Load Kernel Modules. See 'systemctl status systemd-modules-load.service' for details. [ OK ] Started Remount Root and Kernel File Systems. Starting Create Static Device Nodes in /dev... Mounting Kernel Configuration File System... Starting Apply Kernel Variables... Starting Flush Journal to Persistent Storage... [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Mounted Kernel Configuration File System. [ OK ] Started Apply Kernel Variables. [ 5.009889] systemd-journald[92]: Received request to flush runtime journal from PID 1 [ OK ] Reached target Local File Systems (Pre). Mounting /media/ram... [ OK ] Reached target Containers. Mounting /var/volatile... Starting udev Kernel Device Manager... [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started udev Kernel Device Manager. [ OK ] Mounted /media/ram. [ OK ] Mounted /var/volatile. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started udev Coldplug all Devices. [ OK ] Started Load/Save Random Seed. [ OK ] Started Create Volatile Files and Directories. Starting Network Service... Starting Update UTMP about System Boot/Shutdown... [ 5.595190] omap-rproc 55020000.ipu: ignoring dependency for device, assuming no driver [ 5.631142] omap-rproc 55020000.ipu: ignoring dependency for device, assuming no driver Starting Network Time Synchronization... [ 5.647898] omap-rproc 55020000.ipu: assigned reserved memory node ipu2-memory@95800000 [ 5.661346] remoteproc remoteproc0: 55020000.ipu is available [ 5.687983] omap-rproc 40800000.dsp: ignoring dependency for device, assuming no driver [ 5.762742] omap-rproc 40800000.dsp: ignoring dependency for device, assuming no driver [ OK ] Started Update UTMP about System Boot/Shutdown. [ 5.825562] remoteproc remoteproc0: powering up 55020000.ipu [ 5.834764] remoteproc remoteproc0: Booting fw image dra7-ipu2-fw.xem4, size 4395480 [ 5.874738] omap-rproc 40800000.dsp: assigned reserved memory node dsp1-memory@99000000 [ 5.908570] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1 [ 5.940012] remoteproc remoteproc1: 40800000.dsp is available [ 5.958250] remoteproc remoteproc1: Direct firmware load for dra7-dsp1-fw.xe66 failed with error -2 [ 5.967350] remoteproc remoteproc1: powering up 40800000.dsp [ 5.974729] omap-rproc 41000000.dsp: ignoring dependency for device, assuming no driver [ OK ] Started Network Service. [ 6.039184] omap-rproc 41000000.dsp: ignoring dependency for device, assuming no driver [ 6.051553] remoteproc remoteproc1: Direct firmware load for dra7-dsp1-fw.xe66 failed with error -2 Starting Network Name Resolution... [ 6.121837] omap-rproc 41000000.dsp: assigned reserved memory node dsp2-memory@9f000000 [ 6.137291] remoteproc remoteproc1: request_firmware failed: -2 [ 6.139002] remoteproc remoteproc2: 41000000.dsp is available [ 6.203180] remoteproc remoteproc2: Direct firmware load for dra7-dsp2-fw.xe66 failed with error -2 [ 6.224253] remoteproc remoteproc2: powering up 41000000.dsp [ 6.233559] remoteproc remoteproc2: Direct firmware load for dra7-dsp2-fw.xe66 failed with error -2 [ 6.246982] remoteproc remoteproc2: request_firmware failed: -2 [ OK ] Found device /dev/ttyS0. [ 6.294094] Driver for 1-wire Dallas network protocol. [ 6.411271] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2 [ 6.448180] omap-des 480a5000.des: will run requests pump with realtime priority [ 6.478243] omap_hdq 480b2000.1w: OMAP HDQ Hardware Rev 0.:. Driver in Interrupt mode [ OK ] Started Network Time Synchronization. [ 6.531666] virtio_rpmsg_bus virtio0: rpmsg host is online [ OK ] Reached target System Initialization. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activati[ 6.573513] omap_rtc 48838000.rtc: registered as rtc0 on Socket. [ 6.578276] remoteproc remoteproc0: registered virtio0 (type 7) [ 6.587479] remoteproc remoteproc0: remote processor 55020000.ipu is now up [ OK ] Listening on D-Bus System Message Bus Socket. [ 6.664873] virtio_rpmsg_bus virtio0: creating channel rpmsg-proto addr 0x50 [ OK ] Listening on dropbear.socket. [ OK ] Reached target Sockets. [ 6.755364] w1_master_driver w1_bus_master1: Attaching one wire slave 01.000000000000 crc 3d [ OK ] Reached target Basic System. [ 6.791360] net eth0: initializing cpsw version 1.15 (0) Starting TI IPC Daemon... Starting Login Service... Starting rc.pvr.service... [ 6.881605] w1_master_driver w1_bus_master1: Family 1 for 01.000000000000.3d is not registered. [ 6.960493] TI DP83867 48485000.mdio:02: attached PHY driver [TI DP83867] (mii_bus:phy_addr=48485000.mdio:02, irq=POLL) [ 7.001664] phy phy-4a084000.phy.4: Linked as a consumer to regulator.25 [ 7.079563] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ 7.090891] phy phy-4a085000.phy.5: Linked as a consumer to regulator.25 [ 7.122507] net eth1: initializing cpsw version 1.15 (0) [ OK ] Started Launching Vision SDK App. [ 7.156279] libphy: PHY 48485000.mdio:03 not found [ 7.156292] net eth1: phy "48485000.mdio:03" not found on slave 1, err -19 [ 7.199403] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready [ 7.216496] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3 [ OK ] Started D-Bus System Message Bus. [ 7.273455] pvrsrvkm: loading out-of-tree module taints kernel. [ 7.281751] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3 [ 7.296491] omap-aes 4b500000.aes: will run requests pump with realtime priority [ 7.307525] CAN device driver interface [ OK ] Started Daily Cleanup of Temporary Directories. [ 7.342417] ahci 4a140000.sata: controller can't do 64bit DMA, forcing 32bit [ OK ] Reached target Timers. [ 7.359425] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3 [ 7.361703] pvrsrvkm 56000000.gpu: assigned reserved memory node gpu-memory@c0000000 [ OK ] Reached target System Time Synchronized. [ 7.383749] ahci 4a140000.sata: forcing port_map 0x0 -> 0x1 [ 7.385890] omap-aes 4b700000.aes: will run requests pump with realtime priority [ OK ] Started Network Name Resolution. [ 7.412176] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=a7f9dfd6, irq=90) [ 7.425442] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode [ OK ] Started TI IPC Daemon. [ 7.506294] ahci 4a140000.sata: flags: ncq sntf pm led clo only pmp pio slum part ccc apst [ 7.522470] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.gpu on minor 2 [ 7.606050] scsi host0: ahci [ 7.639221] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 79 [ 7.651922] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ] [ OK ] Started rc.pvr.service. [ 8.011283] ata1: SATA link down (SStatus 0 SControl 300) [ 9.794874] NET: Registered protocol family 45 [ 10.164759] cpsw 48484000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx [ 10.172880] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready [ 12.449447] EXT4-fs (nvme0n1p1): recovery complete [ 12.454289] EXT4-fs (nvme0n1p1): mounted filesystem with ordered data mode. Opts: (null) [ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch. [ OK ] Created slice system-systemd\x2dfsck.slice. Starting File System Check on /dev/mmcblk0p1... Starting File System Check on /dev/nvme0n1p1... Starting weston.service... Starting Avahi mDNS/DNS-SD Stack... [ OK ] Reached target Host and Network Name Lookups. [ OK ] Reached target Network. Starting Permit User Sessions... [ OK ] Started File System Check on /dev/mmcblk0p1. [ OK ] Started File System Check on /dev/nvme0n1p1. [ OK ] Started weston.service. [ OK ] Started Permit User Sessions. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Started Serial Getty on ttyS0. [ OK ] Started Getty on tty1. [ OK ] Reached target Login Prompts. Starting Synchronize System and HW clocks... [ 14.493587] DMA: Module install successful, device major num = 240 [ 14.499960] DRV: Module install successful Starting telnetd.service... Mounting /run/media/nvme0n1p1... Mounting /run/media/mmcblk0p1... [ OK ] Started Synchronize System and HW clocks. [ 14.635627] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck. [ OK ] Started telnetd.service. [ OK ] Mounted /run/media/nvme0n1p1. [ OK ] Mounted /run/media/mmcblk0p1. [ OK ] Started Login Service. [ OK ] Reached target Multi-User System. Starting Update UTMP about System Runlevel Changes... [ 14.822948] omap_l3_noc 44000000.ocp: L3 application error: target 3 mod:2 (unclearable) [ 14.831112] omap_l3_noc 44000000.ocp: L3 debug error: target 3 mod:2 (unclearable) [ OK ] Started Update UTMP about System Runlevel Changes. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org dra7xx-evm ttyS0 Arago 2019.09 dra7xx-evm ttyS0 dra7xx-evm login: root root@dra7xx-evm:~# ifconfig eth0 Link encap:Ethernet HWaddr 94:A9:A8:BF:1A:7C inet6 addr: fe80::96a9:a8ff:febf:1a7c/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:2 errors:0 dropped:0 overruns:0 frame:0 TX packets:46 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:328 (328.0 B) TX bytes:7770 (7.5 KiB) Interrupt:87 eth1 Link encap:Ethernet HWaddr 94:A9:A8:BF:1A:7D UP BROADCAST MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 inet6 addr: ::1/128 Scope:Host UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
I checked in the internet and find some related questions, but I cannot find a solution on it.
Could you help me on it? thank you very much!
Qing Zhou