This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Accessing Data and Control UART pins through the 60pin connector

Part Number: IWR6843AOPEVM


Hi,

I want to access both Data and Control UARTs of IWR6843AOPEVM Revision G without using the micro USB. In the forum, it was mentioned that we can use the 'MSS_LOGGER' in the 60-pin connector to read data so I am guessing that is the TX pin of Data UART. Is there any documentation on all the RX/TX pins of both UARTs in the 60-pin connector?

Regards