This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91300: LMP91300SWIFEVM Load2 voltage Swing to 0 to 11.8volt.

Part Number: LMP91300

Hi, 

we design the EVM board For LMP91300 using guidelines according to this ti thread https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/624328/lmp91300-evaluation-board-and-programming-evaluation-board-lmp91300swifevm#2301312.

in this image, load1 is the microcontroller's output, and load 2 net is connected to the microcontroller pin.

My main concern is when all components are soldered without a microcontroller. and power on the board but the point load2 voltage is 11.8V. I am also simulating the same circuit in TINA_TI and same result getting.

is it normal?

because the controller pin's maximum voltage is 4.4 volts.