Hello,
I am new to firmware design, so instead of writing something from scratch, I am looking to adapt an existing demo for my use case. I am wanting to track the location of high reflectivity objects inside a predefined experimental space. The RCS of the object would be maximized using an octahedral corner reflector. The maximum range would be about 15 meters. I need the highest sampling rate and accuracy of position, velocity that I can get. I do NOT need the tracking processing chain at this time, just the 3D positioning and velocity. I need either x,y,z,v or (ideally) azimuth, elevation, distance, velocity.
I see the MRR demo and the SRR demo, however these are not listed as working with the IWR6843AOP. Could these be easily adapted to work with my hardware? I see that I could potentially utilize the people tracking demo as well.
I am rather new to this, so apologies if I am missing something obvious.
Thanks!