Other Parts Discussed in Thread: TMP235, , LM235
I wish to use this part to read temperatures between about -20C and +80C. The data sheet, page 16, figure 18 shows the use of diodes to produce a negative reference. I have read the two related threads on the forum.
It appears from the data sheet that (without the diode offset) 0C gives 0V output and 25C gives 250mV output. Also, -55C will give -550mV output.
What I cannot understand is what temperature will produce 0V with the diode offset. I wonder if this will be -55C?
Thanks.