This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMAG5124-Q1: Hall Sensor

Part Number: TMAG5124-Q1
Other Parts Discussed in Thread: DRV5023-Q1, TMAG5123-Q1

Hi,

TMAG5124G is the current output sensor. Is there any voltage output hall sensor with same Bop & Brp available?

Thanks

  • Hello Bhagyashree,

    Thanks for posting to the sensors forum.

    If you are looking for a unipolar switch an option may be is the DRV5023-Q1, it does not have the exact same threshold offerings as TMAG5124-Q1. The closest options would be 6.9mT and 14.5mT.

    If using an omnipolar switch is an option the TMAG5123-Q1 offers a 10.9mT variant that may be good option for a voltage output device.

    Best,

    Isaac