This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5013-Q1: Absolute Max Rating

Part Number: DRV5013-Q1
Other Parts Discussed in Thread: DRV5013

Hi team,

I have a question. D/S says the B_ max is unlimited. How much tesla will have problem when such strong magnetic field is applied? A few hundred tesla? Theoretical value is okay to close the customer question.

Best Regards,

Shoji

  • Shoji-san,

    Unlike TMR or GMR sensors, Hall-effect elements are not damaged by large input fields.  DRV5013's thresholds are set such that the input field must exceed BOP or BRP to trigger state changes.  When an external field is applied, we can predict the voltage across the Hall-element using this formula:

    VH = (I * B) / (n * e * d)

    where:

    I = applied current

    B = applied external field

    n = charge carrier density

    e = electron charge (1.602e-19)

    d = sensor thickness

    Now, the concern here I think you are raising is what happens to the Hall voltage when our normal input field is increased from 10 mT by 1000 times to something like 10T.  Firstly, there is some limitation to how the material will behave, and it would saturate at very large fields such that we'd stop seeing any increase in voltage.  Secondly, the internal biasing would have to provide the energy to create such a voltage difference across the material and the internal circuits would not be able to generate anything that would result in damage from these extreme cases.  What we should expect to see in such a case is that the voltage clamps to the internal regulation and biasing of the device.

    Thanks,

    Scott

  • Hi Scott,

    So even if extreme MF is applied, the IC cannot be damaged theoretically because of some saturation, right?

    What about big ΔT/Δt?

    Best Regards,

    Shoji

  • Shoji-san,

    Correct, even in extreme magnetic fields we do not anticipate any damage to the sensor.

    For ΔT/Δt, you are asking about how quickly temperature can change without causing damage to the device? 

    Thanks,

    Scott

  • Hi Scott,

    Understood.

    Sorry, I mean ΔB(Tesla)/Δt.

    Best Regards,

    Shoji

  • Hi Shoji-san,

    Scott is currently out of office.

    In regards to your question, as Scott mentioned previously, even in extreme magnetic fields we do not anticipate any damage to the sensor.

    Best regards,

    Jesse

  • Hi Jesse,

    Understood. Thank you for your support!

    Best Regards,

    Shoji