Hello,
I'm using the TUSS4470 in the pre-driver mode with a transformer.
Since the peak voltage on the secondary circuit reaches 1400 V I recalculated the capacitance on the INP pin using the formula found on the forum:
INP_Impedance = R_INP + [ 1 / ( 6.28 * f_burst * C_INP ) ]
To have a current of 10 mA with a burst frequency of 235 KHz it is necessary to reduce the capacitance from 330pF (value indicated in the datasheet) to 47pF.
Therefore I measured the Vout level with LNA gain = 20 V/V, first and last logamp stages both enabled; by reducing Cinp from 330pF to 47pF the Vout pedestal level increases from 390 mV to 500 mV. Since I need to detect very small signals, losing 110 mV is quite annoying.
Is it possible to compensate for this effect in some way?
Am I using an excessively low Cinp value?
By the way, Cinn was set to 18.1 nF by applying the formula reported in the datasheet.
Thanks,
Paolo