Other Parts Discussed in Thread: UNIFLASH,
I have used UNIFLASH and loaded DEVRAM file but during verification I am getting the following error. How to rectify this error kindly help me.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Saravanan Sunderesan,
I have not used UNIFLASH to actually flash the PGA970. Are you using the PGA970EVM? And if so, have you tried using the GUI to download the firmware hex file? I will have to attempt this myself to see what may be going on, but it would appear that the M0 is actually running instead of reset which may prevent the firmware from being able to be verified.
Best regards,
Bob B
Hi Saravanan Sunderesan,
I was able to download and verify as shown below:
This was a hex file I generated in CCS. I also was able to load and verify the example generic hex file. You may have incorrect settings in the .ccxml setup file for the debugger.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/1023/PGA970.ccxml
You can try and use this attached setup file instead. Or you can try setting up your own by clicking the Edit button before selecting Start. The configuration should be like shown below:
Best regards,
Bob B