Other Parts Discussed in Thread: HDC2010, TMP116, OPT3001
Hi,
I am having trouble getting the HDC2010 to send me an ACK after writing over it's address. I have hooked up the other two sensors TMP116 and OPT3001 successfully, and have received ACKs from both and retrieved their device IDs to know communication is working. I have hooked up the H_V+ pin to the 3.3V pin and am trying to communicate to the address 0x40, however, after I send the address I receive no acknowledgement from the device. I've used a protocol analyzer and have seen then NAK as well. Would I be able to get some help navigating this? Thank you.