Other Parts Discussed in Thread: IWR1843
Hello,
1, Solidify xwr18xx_mmw_demo.bin in sdk3.5(D:\SoftWare\ccs11_2\software\mmwave_sdk_03_05_00_04\packages\ti\demo\xwr18xx) into the iwr1843 board
2, use the mmWave_Demo_Visualizer. If the mmWAVe_demo_visualizer is used, the function can run properly if the default configuration is used. The default configuration is as follows:
3, I modify the parameters as follows, the program can run,
4, the program can not work if the green 512 selected in the above figure is changed to 1024, but if the AD sampling number is changed to 1024 and the rx channel number is changed to 2, the program can run. I suspect the problem is out of memory, but I don't know how to determine if it is memory and fix it
Regards,
Gary