This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI experts,
I am trying to implement a program that boots the radar via the SPI connection from PC to an 6843AOP or 6432L EVM. Our plan is to disable its QSPI flash first and then use FTDI interface to do the job.
Would you please suggest where we can get started quickly, which code or document in the radar toolbox in particular? Or it would be really appreciated if a template code is available for this.
Best regards,
Tony
Hi Tony,
Please see this application note IWR6843 Bootloader Flow (ti.com)
There is a section there on SPI-based booting mode in our x843 devices. Hope this helps.
Regards,
Tim
Hi Tony,
The only reference that may be helpful is in this discussion:
Another potentially relevant thread:
I'd recommend searching for other relevant E2E posts that might be on the same topic as well.
I'm closing this thread for now.
Regards,
Tim