Other Parts Discussed in Thread: LMT70A, SN74AUP1G04, LMT70
Hi
we are in the process of developing a breakout board for testing our use case probe model, incorporating both LMT70A and TMP117 sensors. Our objective is to achieve an accuracy of 0.1°C, ensuring compatibility with various MCUs such as Arduino, ESP32, and STM32. I have attached the schematic diagrams for both sensors. Your feedback on these designs would be highly appreciated.
**LMT70A:** https://drive.google.com/file/d/1j2MVZp0KV-FrCBKdv6_HK51-misFT5Ha/view?usp=sharing
Equipped with two LMT70A analog temperature sensors – one for body temperature and one for ambient temperature. Both sensors are connected to two separate ADC channels, each featuring a 12-bit built-in ADC channel in the MCU. The temperature measurement range spans from 20°C to 42°C. The operating voltage for the system is 3.3V. Could you please review the schematic to confirm its accuracy? Additionally, with this schematic, is an accuracy of 0.1 achievable or not?
**TMP117:** https://drive.google.com/file/d/1m_Z95TNhb_sLXOfgleLUPCUVH2t3JZa1/view?usp=sharing
Equipped with two TMP117 digital temperature sensors – one for body temperature and one for ambient temperature. Both sensors are connected to two separate I2C channels in one MCU. The temperature measurement range spans from 20°C to 42°C. The operating voltage for the system is 3.3V. Could you please review the schematic to confirm its accuracy? Additionally, with this schematic, is an accuracy of 0.1 achievable or not?
Is the U3 and U4 (SN74AUP1G04) component needed in the alert pin? Also, want to know the purpose of the alert pin?
Your expertise and insights will be invaluable in refining our designs.
Thank you,
Best Regards