This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM96000: could the device support the highest speed requirement when there are multi master devices?

Part Number: LM96000
Other Parts Discussed in Thread: LM96194, LM111

Hi,

Below is my customer design concept.

I'm going to propose LM96000x2 or LM96194*2 due to the device only support up to 3xPWM and 2xPWM.

As you see there are 4 host could send command to fan control to control fan speed.

My question is could our fan control only work as the highest speed from these 4 masters?

I mean when the 4 masters send different speed to fan control, could fan control only operate the highest one?