Other Parts Discussed in Thread: , AWR2944EVM
Hi, I have a question related to crystal oscillator.
I would like to create a platform to implement the prototype of the automotive radar using AWR2544. It is understood that a crystal clock source of 40 MHz or 50 MHz can be used, and we can see that several requirements are written on the datasheet. If I want to use it for a automotive application, do I have to attach an auto-certified product (crystal source)?
Or, can any product be used if all the information on the datasheet is satisfied?
Also, if possible, can you recommend between 40 MHz and 50 MHz?
I would like to know about criteria about crystal's frequency selection. (e.g. , low price, related to functional safety, dependence on design process, etc.)
Thanks in advance.