This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMCS1133: Sensors forum

Part Number: TMCS1133
Hi Team,
Greetings of the Day!
We are evaluating TMCS1133B1A (Hall-effect Current Sensor), which has a Signal bandwidth of 1 MHz.

Now we are testing the input-to-output response at 150KHz frequency, which is less than the rated bandwidth. Here we are getting a typical response of nearly 1.6usec, between the input to output waveforms.

Here we are sharing the testing observations. Pls verify these and share your suggestion to improve the response time.

DSO Image:
Yellow: Current sensor input (50mV/A), Dark_Blue: Current sensor output.


Practical Observations:
Current sensor input = 16A Peak (32A p-p).
Current sensor output = 20A Peak (40A p-p).

Thank You in advance!
Regards,
Chaithanya.