Hello, page 62 of the datasheet lists the available interrupt modes, which can be set by the "INT_MODE[2:0]" bits of register "INT_Config_1." I am unclear on the difference between the "Interrupt through INT" mode (1h) and the "Interrupt through INT and ignore if I2C communication active with the Target" mode (2h). Could you please provide a clarification and use cases where one is used versus the other? Thank you.