This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMAG5231: BOP and BRP Threshold and Release Operate Point production variation data?

Part Number: TMAG5231

I am using the TIMSS tool to characterize the performance of the TMAG5231C1DQDBZR sensor when using an N52 axial cylindrical magnet in a hinge application. In addition to nominal conditions, I am using the tool to simulate edge cases, exploring tolerance ranges of key parameters: relative position, magnet size, strength and temperature, and sensor BOP and BRP. Per the TMAG5231 specification, I am using the specified min or max values of each threshold for worst case conditions. However, to better quantify PPM failure rates, I need production variation data for BOP and BRP such as standard deviation or sigma level. Is this data available?