- If a VOUT of EN > H product and VOUT of EN < L product are connected to the same output line, will the output voltage be VQ at B=0MT? (Datasheet 9.1.4 Design with multiple sensors)
- Does ROUT affect the output voltage of the product? (Couldn't confirm the ROUT formula on the datasheet.) What is ROUT used for?
- It says in the DS(8.4) that "When the EN pin is tied to GND, the TMAG5253 enters an ultra-low power shutdown mode that consumes only 20-nA current. During the shutdown mode, the OUT pin is driven to a high-impedance state.". Could you explain what kind of state is high-impedance state?