Tool/software:
Dear Sir,
The MMWAVE SDK User Guide states that I can perform a phase shift on three TX antennas by changing the <txPhaseShifter>
parameter in the configuration file.
Furthermore, the document "Beamforming_in_LRPD.pdf" provides a MATLAB script as an example for calculating the <txPhaseShifter>
parameter necessary for beamforming, using a one-dimensional antenna array indexed as m_ind = [0 1 2].
If I want to implement beamforming on the AWR6843AOP as well, I am wondering if there is a similar MATLAB script available to calculate the control numbers for the AWR6843AOP antenna array.
Sincerely,
HC.Chang