This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC2022: Measuring humidity at negative temperatures

Part Number: HDC2022

Tool/software:

Could the HDC2022 be used to measure humidity at negative temperatures? Which is humidity range expected at the situation? Could the sensor return negative humidity? Does Texas have humidity errors percentage at negative temps?

Best regards,

Leonardo

  • Leonardo,

    HDC2022 will read RH at negative temperatures, but the RH accuracy below 0C is not characterized or guaranteed. The sensor will not report negative humidity, that is not possible. The sensor will report a range from 0% to 100% RH. It is possible to have a relative humidity level at negative temps if there is still moisture in the air, but we do not have min/max or typical data for humidity below 0C.

    Regards

    -Alex Thompson