Other Parts Discussed in Thread: UNIFLASH
Tool/software:
We designed a board based on AWR1843BOOST, basically we did not populate onboard XDS110 and some other irrelevant parts and added a connector for XDS110. We brought the following signal out to XDS110 connector.
XDSSET_TMS(N10) / XDSET_TCK(P10) / XDSET_TDO(N13) / XDSET_TDI(R11) / AR_NRST_XDS(R3) / 3.3V / GND.
And we also update the our external XDS110 firmware to 3.0.0.29
And put the custom board to flashing mode on SOP switch (101) but it did not flash using uniflash.
but same procedure works on actual AWR1843BOOST (with same internal xds110 firmware 3.0.0.29), is there any other setting we need to consider?
any help greatly appreciated.