Tool/software:
Hi there
I have a question in AWRL1432_ADAS_BSD_DEMO_v2.0.
We just want to know in BSD Extend Vmax function is support RDmap function?
In config, we turn on
guiMonitor 2 1 0 0 1 1 0 0 1 0 0
In the number 5 place is RDmap enable, and number 2 place is range profile enable.
We saw in ccs code have function to using RD map, then when we check and do experiment, we get the range is correct but doppler is wrong.
the doppler part, half are zero values in doppler bins and MATLAB analyze surf figure like follow:
our engineer analyze, and turn on range profile function to compare between with RD map, there where have the same of single performance in range bins. (figure as follow)
RD map (x is range, y is single value)
Range profile
But speed(doppler) is wrong because we recorded data in RD map, half are zero values in doppler bins.
Now, the first question is how can we solve this or it's not support using RD map function?
second, the scaling function in range profile is 20*log10(data), does the TI team have RD map's scaling function?
third, in the detect point, we can get the point information like SNR and Noise, but the target's Amp(SNR + Noise) single is too different with range profile's single.
Thank you,
Leo Lin