This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: SDK version 05_04_00_01
Hi team ,
i am using the latest SDK version 05_04_00_01, So i have some questions that is
1) I want to know is there any MCAN API available which can remove a message from the RX queue.
2) And also is there any API available which can show what are all the messages there / stored currently in the RX queue ?
I just searched through the SDK but i am not able find it out , so it will be grateful if you can give some insights on this !!
Thanks
Hello,
Thanks for reaching out regarding your questions on the CAN driver. One of engineers will reply within the next two business days.
Thank you for your patience,
Kristien
Hi ,
I am still waiting for the reply. I haven't received anything yet and hope to hear back soon
Thanks ...
Hello.
Apologies for the delay in response. There is no API that explicitly removes the message from the RX queue. This would not be required as you can use filtering via a message filter to remove any unwanted message and the buffer only has messages you want to read/receive.
Sincerely,
Santosh