Tool/software:
Hi,
Greetings...
I have gone through the datasheet of AFE3010. In the application diagram, I have seen that the phase of AC is directly connected to bridge rectifier (a resistor is connected for current limiting) & given to the VDD of the IC.
From the specs, I understand that the max. voltage of VDD is 26V & this IC used in 230V & 120V AC applications.
As per my understanding, the input AC needs to be stepped down before rectifying. If AC step down isn't there, then the input AC will be rectified. For example, 120V AC will be available as ~170V DC after rectification.
Kindly guide me in understanding how the AC is stepped down in the circuit shown in the application diagram of AFE3010 IC.
Best Regards,
Prahaladh S