Tool/software:
Hi,teams.
I measured the signal strength under the following two conditions by modifying the variables in the sample file "chirp_60G_6m.lua".
Condition 1: Configuration assuming CW transmission from Tx1
h_TxChCtrlBitMask=1
c_ChirpTxMimoPatSel=0
c_FrameTrigMode=4
Condition 2: Configuration assuming CW transmission from Tx2
h_TxChCtrlBitMask=2
c_ChirpTxMimoPatSel=0
c_FrameTrigMode=4
The result showed that the signal strength in Condition 1 is more than 20dB higher than the signal strength in Condition 2.
I had assumed that the signal strengths in both conditions would be the same, so if there is a mistake in the configuration, please let me know.