Other Parts Discussed in Thread: LDC1001
Tool/software:
Hi all, I am using the TI LDC 1001-Q1 as proximity sensor to detect metallic objects. The LDC is connected to a Microcontroller and to an external squared coil with an inductance of 220uH (inner diameter/ outer diameter = 0.86). The input capacitor is 10nF, resulting in an LC frequency of about 105 kHz. The LDC together with the microcontroller and other components, are soldered in a PCB, being only the coil external.
In our application the proximity data is about 4500 when no metal object is on top , and Rp of about 8KOhm. When a metallic object is on top at about 10cm, the Rp drops at around 7kOhm. The usual working register LDC status is 48.
However, we noticed 2 anomalies in production on some of our sensors:
1) Some sensors at some point without any apparent reason transmit a status of 0, with Rpmin and Rpmax registers at 0 as well, and the Rp goes at 60352, and then they go in a condition with Rp=Rpmax. Basically our application was working fine since 2 weeks, with status 48, Rp around 8k, and all of a sudden we got this status 0 and Rp=60352, and from that instant on it was always in Rpmax with sense status of 240, so not working anymore.
2) At some point, after a couple of weeks of good behaviour, without any changes in the external condition, the Rp quickly starts to decrease in about few hours, from nominal 8k (in case no metallic object) down to 2k (in case of no metallic object), and therefore our thresholds and system do not work anymore, and the sensor show a permanent change of regime.
Please could you help us in fixing these issues in production?
Please let me know,
Thank you,
Best regards,
Donato.