This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWRL6432AOPEVM: Hardcoded Config using CLI_BYPASS

Part Number: AWRL6432AOPEVM
Other Parts Discussed in Thread: AWRL6432

Tool/software:

Hello TI-Team,

i want to add Hardcodedconfig to my device. I made following changes to the Code and flashed the device:

#define CLI_BYPASS 1
//conveyor_belt_true_ground_speed_5m_60GHz.cfg
#define MAX_RADAR_CMD 21
char *radarCmdString[MAX_RADAR_CMD] = {
    "sensorStop 0 \n\r",
    "chirpComnCfg 16 0 0 128 4 28 0 \n\r",
    "chirpTimingCfg 28 32 0 40 60.5 \n\r",
    "channelCfg 7 3 0 \n\r",
    "frameCfg 2 0 400 64 100 0 \n\r",
    "antGeometryCfg 0 0 1 1 0 2 0 1 1 2 0 3 \n\r",
    "guiMonitor 1 1 0 0 0 1 0 0 0 0 0 \n\r",
    "sigProcChainCfg 64 32 1 0 0 0 0 0 \n\r",
    "sensorPosition 0 0 0.3 0 0 \n\r",
    "cfarCfg 2 8 4 3 0 10.0 0 0.95 0 1 1 1 \n\r",
    "aoaFovCfg -20 20 -40 40 \n\r",
    "rangeSelCfg 0.1 5.0 \n\r",
    "clutterRemoval 1 \n\r",
    "compRangeBiasAndRxChanPhase 0.0 1.00000 0.00000 -1.00000 0.00000 1.00000 0.00000 -1.00000 0.00000 1.00000 0.00000 -1.00000 0.00000 \n\r",
    "adcDataSource 0 C:\\\\ti\\\\Workarea\\\\Uploads\\\\mmwave_lp_sdk\\\\examples\\\\datapath\\\\common\\\\testBench\\\\major_motion\\\\adc_data_0001_CtestAdc6Ant.bin \n\r",
    "adcLogging 0 \n\r",
    "lowPowerCfg 1 \n\r",
    "factoryCalibCfg 0 0 40 0 0x1ff000 \n\r",
    "configRANSAC 1 200 1.0 \n\r",
    "baudRate 1250000 \n\r",
    "sensorStart 0 0 0 0 \n\r",
};

It is possible to connect COM Port in IndustrialVisualizer , but i cannot see the Data Stream using "Start without sending config file".

Do i have to change the Python Code?Baudrate for example? (in Putty it shows continues data but only not readable special characters...)

thank you very much :)