Other Parts Discussed in Thread: IWR6843AOPEVM, UNIFLASH
Tool/software:
Howdy,
Having some problems with the MMWAVEICBOOST + IWR6843AOPEVM.
I can power on the IWR6843AOPEVM and run the web demo with no issues. The dual CP2105 USB ports are easily recognized. Used the included micro USB cable.
When adding the MMWAVEICBOOST, things are not working correctly. I am able to connect the FTDI connection to the computer with no issues.
The board state is attached here when plugged into the FTDI micro-usb port.
When I connect only to the XDS micro-usb (with the same cable), I am left with no devices detected, and the following board state:
I ensured that the S3 on the IWR6843AOPEVM was in the off state. Again, the IWR6843AOPEVM is working on demo, but the MMWAVEICBOOST + IWR6843AOPEVM is not able to be detected by MMWave Studio or Uniflash.
I have tried three different power supplies, all 5V.
I followed the below thread as well, nothing here worked for me.
https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1303822/mmwaveicboost-not-working
Please advise,
Tomas