This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6243: TDM implementation for 2-chip cascade radar (IWR6243)

Part Number: IWR6243


Tool/software:

Hi,

I am working on implementing the TDM for the IWR6243 cascade sensor. Currently, we have the DDMA implementation from the Sitara SDK for this cascade configuration. I have modified the chirpCfg to ensure that only one transmitter is enabled at a time. However, I want to ensure that the chirp sequence in each frame follows this specific TDM order:

[Master_Tx1, Master_Tx2, Master_Tx3, Slave_Tx1, Slave_Tx2, Slave_Tx3, Master_Tx1, ...]

My concern is that with the modifications I made in chirpCfg, there might still be overlapping activations, where the Master's Tx1 and the Slave's Tx1 are enabled simultaneously, followed by simultaneous chirps from Master's Tx2 and Slave's Tx2, and so on.

Is there a TDM implementation or guidance available specifically for a 2-chip cascade radar setup to achieve the desired TDM chirp sequence?

Regards,

Attiya