This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443BOOST:AWR 1443 Boost功能:Hardware trigger mode

Part Number: AWR1443BOOST
Other Parts Discussed in Thread: AWR1443

Tool/software:

Hello, I want to use AWR1443BOOST+DCA1000 to use the hardware trigger mode. According to the discussion in the forum before, I have welded the R62 resistance and connected it to the microcontroller which can send a pulse with a period of 50ms and a width of 2us as shown in the following picture.

The configuration for mmwave studio is as follows:

The first question is: what is the flow using hardware triggering? If I set No of Frames to 401, then click on DCA1000 ARM and Trigger Frame in turn. After triggering, should a pulse trigger all 401 frames or a pulse trigger only one frame and generate a bin file only after all 401 pulses have been sent?
The second problem is that when I click the DCA1000 ARM and Trigger Frame in turn according to the circuit connection as shown above, the data as shown below is still received without pulse input, but there is only one frame of data

After I clicked the DCA1000 ARM and Trigger Frame again and gave the pulse, the following error occurred and no data was received.

How can these two problems be solved? Thank you very much!

  • Hi,

    Please find my comments below. 

    The first question is: what is the flow using hardware triggering? If I set No of Frames to 401, then click on DCA1000 ARM and Trigger Frame in turn. After triggering, should a pulse trigger all 401 frames or a pulse trigger only one frame and generate a bin file only after all 401 pulses have been sent?

    All frames are to be triggered by HW pulse. Trigger frame tab is required to be used once only to indicate the start. 

    The second problem is that when I click the DCA1000 ARM and Trigger Frame in turn according to the circuit connection as shown above, the data as shown below is still received without pulse input, but there is only one frame of data

    For this can you once click the DCA 1000 ARM tab, Triger frame tab and then provide all the required sync in pulses for all the frames. With this you should have all the data for all the frames. 

    Thanks,

    Pradipta.

  • Hi, Pradipta.

    Thank you very much for your answer.
    In response to your answer to the first question, can I understand it as: When I need a bin file with 401 Frames, I just need to change the No of Frames in mmwave Studio to 401, then click DCA1000 ARM tab and Trigger Frame tab. Is it enough to input 401 pulse signals into SYNC_IN?
    In response to your answer to the second question, I still don't understand why I click the DCA1000 ARM tab and Trigger Frame tab in turn, but no signal is input to SYNC_IN, but a frame of data is still generated?
    I also have a question: how do I know when my data collection is over? After the previous data collection and the message "Record is completed. Record stop is done successfully." I click the DCA1000 ARM tab and Trigger Frame tab one by one again, and "Frames are already triggered for the device" will be displayed, and the data will not be received if I continue to give the pulse signal. Can you tell me what I should do?
    Thank you very much,
    Lu Datong.

  • Hi,

    In response to your answer to the first question, can I understand it as: When I need a bin file with 401 Frames, I just need to change the No of Frames in mmwave Studio to 401, then click DCA1000 ARM tab and Trigger Frame tab. Is it enough to input 401 pulse signals into SYNC_IN?
    In response to your answer to the second question, I still don't understand why I click the DCA1000 ARM tab and Trigger Frame tab in turn, but no signal is input to SYNC_IN, but a frame of data is still generated?

    I do not see this on the bench. Can you send across your lua script so that i can try and reproduce that. 

    Thanks,

    Pradipta.

  • Hi, Pradipta. Thank you very much for your answer.
    The following code is my lua script, can you suggest some solutions to my above problems based on this script?
    ar1.SOPControl(2)
    ar1.Connect(3,115200,1000) --first num is Application/User UART id

    --BSS and MSS firmware download
    info = debug.getinfo(1,'S');
    file_path = (info.source);
    file_path = string.gsub(file_path, "@","");
    file_path = string.gsub(file_path, "DataCapture.lua","");
    fw_path = file_path.."..\\..\\rf_eval_firmware"

    --Export bit operation file
    bitopfile = file_path.."\\".."bitoperations.lua"
    dofile(bitopfile)

    --Read part ID
    --This register address used to find part number for ES2 and ES3 devices
    res, efusedevice = ar1.ReadRegister(0xFFFFE214, 0, 31)
    res, efuseES1device = ar1.ReadRegister(0xFFFFE210, 0, 31)
    efuseES2ES3Device = bit_and(efusedevice, 0x03FC0000)
    efuseES2ES3Device = bit_rshift(efuseES2ES3Device, 18)

    --if part number is zero then those are ES1 devices
    if(efuseES2ES3Device == 0) then
    if (bit_and(efuseES1device, 3) == 0) then
    partId = 1243
    elseif (bit_and(efuseES1device, 3) == 1) then
    partId = 1443
    else
    partId = 1642
    end
    elseif(efuseES2ES3Device == 0xE0 and (bit_and(efuseES1device, 3) == 2)) then
    partId = 6843
    ar1.frequencyBandSelection("60G")
    --if part number is non-zero then those are ES12 and ES3 devices
    else
    if(efuseES2ES3Device == 0x20 or efuseES2ES3Device == 0x21 or efuseES2ES3Device == 0x80) then
    partId = 1243
    elseif(efuseES2ES3Device == 0xA0 or efuseES2ES3Device == 0x40)then
    partId = 1443
    elseif(efuseES2ES3Device == 0x60 or efuseES2ES3Device == 0x61 or efuseES2ES3Device == 0x04 or efuseES2ES3Device == 0x62 or efuseES2ES3Device == 0x67) then
    partId = 1642
    elseif(efuseES2ES3Device == 0x66 or efuseES2ES3Device == 0x01 or efuseES2ES3Device == 0xC0 or efuseES2ES3Device == 0xC1) then
    partId = 1642
    elseif(efuseES2ES3Device == 0x70 or efuseES2ES3Device == 0x71 or efuseES2ES3Device == 0xD0 or efuseES2ES3Device == 0x05) then
    partId = 1843
    elseif(efuseES2ES3Device == 0xE0 or efuseES2ES3Device == 0xE1 or efuseES2ES3Device == 0xE2 or efuseES2ES3Device == 0xE3 or efuseES2ES3Device == 0xE4) then
    partId = 6843
    ar1.frequencyBandSelection("60G")
    else
    WriteToLog("Inavlid Device part number in ES2 and ES3 devices\n" ..partId)
    end
    end

    --ES version
    res, ESVersion = ar1.ReadRegister(0xFFFFE218, 0, 31)
    ESVersion = bit_and(ESVersion, 15)

    -----------------------ADC_Data file path--------------------------

    --data_path = file_path.."..\\PostProc"
    --adc_data_path = "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\PostProc\\adc_data.bin"

    data_path = "D:\\LDT\\Data\\Action"
    adc_data_path = "D:\\LDT\\Data\\adc_data.bin"

    -- Path above mentioned can be changed according to your requirements

    -- Download Firmware
    if(partId == 1642) then
    BSS_FW = fw_path.."\\radarss\\xwr16xx_radarss.bin"
    MSS_FW = fw_path.."\\masterss\\xwr16xx_masterss.bin"
    elseif(partId == 1243) then
    BSS_FW = fw_path.."\\radarss\\xwr12xx_xwr14xx_radarss_ES2.0.bin"
    MSS_FW = fw_path.."\\masterss\\xwr12xx_xwr14xx_masterss_ES2.0.bin"
    elseif(partId == 1443) then
    BSS_FW = fw_path.."\\radarss\\xwr12xx_xwr14xx_radarss.bin"
    MSS_FW = fw_path.."\\masterss\\xwr12xx_xwr14xx_masterss.bin"
    elseif(partId == 1843) then
    BSS_FW = fw_path.."\\radarss\\xwr18xx_radarss.bin"
    MSS_FW = fw_path.."\\masterss\\xwr18xx_masterss.bin"
    elseif(partId == 6843) then
    BSS_FW = fw_path.."\\radarss\\xwr68xx_radarss.bin"
    MSS_FW = fw_path.."\\masterss\\xwr68xx_masterss.bin"
    else
    WriteToLog("Invalid Device partId FW\n" ..partId)
    WriteToLog("Invalid Device ESVersion\n" ..ESVersion)
    end

    -- Download BSS Firmware
    if (ar1.DownloadBSSFw(BSS_FW) == 0) then
    WriteToLog("BSS FW Download Success\n", "green")
    else
    WriteToLog("BSS FW Download failure\n", "red")
    end

    -- Download MSS Firmware
    if (ar1.DownloadMSSFw(MSS_FW) == 0) then
    WriteToLog("MSS FW Download Success\n", "green")
    else
    WriteToLog("MSS FW Download failure\n", "red")
    end

    -- SPI Connect
    if (ar1.PowerOn(1, 1000, 0, 0) == 0) then
    WriteToLog("Power On Success\n", "green")
    else
    WriteToLog("Power On failure\n", "red")
    end

    -- RF Power UP
    if (ar1.RfEnable() == 0) then
    WriteToLog("RF Enable Success\n", "green")
    else
    WriteToLog("RF Enable failure\n", "red")
    end

    ---------------------------Channel & Adc Config---------------------------
    -- Tx, Rx, adcbits, outputfmt, cascading
    if (ar1.ChanNAdcConfig(1, 1, 1, 1, 1, 1, 1, 2, 1, 0) == 0) then
    WriteToLog("ChanNAdcConfig Success\n", "green")
    else
    WriteToLog("ChanNAdcConfig failure\n", "red")
    end

    if (partId == 1642) then
    -------------LP Mode--------------
    if (ar1.LPModConfig(0, 1) == 0) then
    WriteToLog("LPModConfig Success\n", "green")
    else
    WriteToLog("LPModConfig failure\n", "red")
    end
    else
    if (ar1.LPModConfig(0, 0) == 0) then
    WriteToLog("Regualar mode Cfg Success\n", "green")
    else
    WriteToLog("Regualar mode Cfg failure\n", "red")
    end

    -------------RF LDO Bypass-------------
    if (ar1.RfLdoBypassConfig(0x3) == 0) then
    WriteToLog("RfLdoBypass Cfg Success\n", "green")
    else
    WriteToLog("RfLdoBypass Cfg failure\n", "red")
    end
    end

    if (ar1.RfInit() == 0) then
    WriteToLog("RfInit Success\n", "green")
    else
    WriteToLog("RfInit failure\n", "red")
    end

    RSTD.Sleep(1000)

    if (ar1.DataPathConfig(1, 1, 0) == 0) then
    WriteToLog("DataPathConfig Success\n", "green")
    else
    WriteToLog("DataPathConfig failure\n", "red")
    end

    if (ar1.LvdsClkConfig(1, 1) == 0) then
    WriteToLog("LvdsClkConfig Success\n", "green")
    else
    WriteToLog("LvdsClkConfig failure\n", "red")
    end

    if((partId == 1642) or (partId == 1843) or (partId == 6843)) then
    if (ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0) == 0) then
    WriteToLog("LVDSLaneConfig Success\n", "green")
    else
    WriteToLog("LVDSLaneConfig failure\n", "red")
    end
    elseif ((partId == 1243) or (partId == 1443)) then
    if (ar1.LVDSLaneConfig(0, 1, 1, 1, 1, 1, 0, 0) == 0) then
    WriteToLog("LVDSLaneConfig Success\n", "green")
    else
    WriteToLog("LVDSLaneConfig failure\n", "red")
    end
    end

    -- if (ar1.SetTestSource(4, 3, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0, 0, 0, 0, -327, 0, -327,
    -- 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0) == 0) then
    -- WriteToLog("Test Source Configuration Success\n", "green")
    -- else
    -- WriteToLog("Test Source Configuration failure\n", "red")
    -- end

    -------------------------------------ProfileConfig-------------------------------------
    if((partId == 1642) or (partId == 1843)) then
    if(ar1.ProfileConfig(0, 77, 10, 6, 65, 0, 0, 0, 0, 0, 0, 74.978, 0, 521, 9121, 0, 0, 30) == 0) then
    WriteToLog("ProfileConfig Success\n", "green")
    else
    WriteToLog("ProfileConfig failure\n", "red")
    end
    elseif((partId == 1243) or (partId == 1443)) then
    if(ar1.ProfileConfig(0, 77, 7, 3.66, 56.9, 0, 0, 0, 0, 0, 0, 70.295, 0, 256, 5000, 0, 0, 30) == 0) then
    WriteToLog("ProfileConfig Success\n", "green")
    else
    WriteToLog("ProfileConfig failure\n", "red")
    end
    elseif(partId == 6843) then
    if(ar1.ProfileConfig(0, 60.25, 200, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 128, 10000, 0, 131072, 30) == 0) then
    WriteToLog("ProfileConfig Success\n", "green")
    else
    WriteToLog("ProfileConfig failure\n", "red")
    end
    end
    -------------------------------------ChirpConfig-------------------------------------

    if (ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0) == 0) then --(100)tx0
    WriteToLog("ChirpConfig Success\n", "green")
    else
    WriteToLog("ChirpConfig failure\n", "red")
    end

    if (ar1.ChirpConfig(1, 1, 0, 0, 0, 0, 0, 0, 1, 0) == 0) then --(010)tx1
    WriteToLog("ChirpConfig Success\n", "green")
    else
    WriteToLog("ChirpConfig failure\n", "red")
    end

    if (ar1.ChirpConfig(2, 2, 0, 0, 0, 0, 0, 0, 0, 1) == 0) then
    WriteToLog("ChirpConfig Success\n", "green")
    else
    WriteToLog("ChirpConfig failure\n", "red")
    end
    -------------------------------------FrameConfig-------------------------------------
    if (ar1.FrameConfig(0, 2, 401, 1, 50, 0, 0, 2) == 0) then
    WriteToLog("FrameConfig Success\n", "green")
    else
    WriteToLog("FrameConfig failure\n", "red")
    end

    -- select Device type
    if (ar1.SelectCaptureDevice("DCA1000") == 0) then
    WriteToLog("SelectCaptureDevice Success\n", "green")
    else
    WriteToLog("SelectCaptureDevice failure\n", "red")
    end

    --DATA CAPTURE CARD API
    if (ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098) == 0) then
    WriteToLog("CaptureCardConfig_EthInit Success\n", "green")
    else
    WriteToLog("CaptureCardConfig_EthInit failure\n", "red")
    end
    --AWR12xx or xWR14xx-1, xWR16xx or xWR18xx or xWR68xx- 2 (second parameter indicates the device type)
    if ((partId == 1642) or (partId == 1843) or (partId == 6843)) then
    if (ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30) == 0) then
    WriteToLog("CaptureCardConfig_Mode Success\n", "green")
    else
    WriteToLog("CaptureCardConfig_Mode failure\n", "red")
    end
    elseif ((partId == 1243) or (partId == 1443)) then
    if (ar1.CaptureCardConfig_Mode(1, 1, 1, 2, 3, 30) == 0) then
    WriteToLog("CaptureCardConfig_Mode Success\n", "green")
    else
    WriteToLog("CaptureCardConfig_Mode failure\n", "red")
    end
    end

    if (ar1.CaptureCardConfig_PacketDelay(25) == 0) then
    WriteToLog("CaptureCardConfig_PacketDelay Success\n", "green")
    else
    WriteToLog("CaptureCardConfig_PacketDelay failure\n", "red")
    end

    --Start Record ADC data
    ar1.CaptureCardConfig_StartRecord(adc_data_path, 1)
    RSTD.Sleep(1000)

    Thanks,

    Datong Lu.

  • Hi Datong,

    Can you confirm once if you use the SW trigger instead of H/W trigger does it work at your end. Do you receive proper ADC data in that case. 

    Thanks,

    Pradipta.

  • Hi, Pradipta.

    Thank you very much for your patient answer.
    What I can confirm is that I received the correct ADC data when I used the software trigger. When I use hardware trigger, there is no wire inserted into the SYNC_IN port, there is no data reception, when the wire is inserted, regardless of whether there is an external signal input in the pipeline, there will be a frame of data reception, that is to say, once the wire is inserted, there will be a frame of data reception, regardless of whether there is a high or low level in the line. (This is in the case of AWR1443 and MCU common ground operation).
    How should this be solved?
    Thanks,
    Datong Lu.

  • Hi Datong,

    Can you once solder the wire to the Sync in port and provide a pulse train on that channel. With this can you let me know if you receive the complete frame data or not?

    Thanks,

    Pradipta.