TMP451-Q1: TMP451 detects OPEN FAULT after initialization

Part Number: TMP451-Q1
Other Parts Discussed in Thread: TMP451, , TMP461

Tool/software:

Hi TI Expert,

We encounter a low probability failure problem: After the system is powered on, the TMP451 detects the OPEN Fault (Reg 0x02 = 0x84, bit 2 = 1) after initialization and assert the ALERT pin. The failure disappears after the system is restarted, and the probability of recurrence is very low.

To initialize TMP451, the following registers are written after power on :

Setup Write to [0x4C] + ACK
0x09+ACK
0x40+ACK
Setup Wrte to [0x4C]+ACK
0x03+ACK
0x40+ACK
Setup Write to [0x4C] + ACK
0x19+ACK
0xBF + ACK
Setup Write to [0x4C] + ACK
0x20+ACK
0xFE + ACK
Setup Write to [0x4C] + ACK
0x11 + ACK
0xFC+ACK
Setup Wrte to [0x4C] + ACK
0x0D+ACK
0xA9 + ACK
Setup Wrte to [0x4C] + ACK
0x0B + ACK
0xFF + ACK
Setup Write to [0x4C] + ACK
0x09+ACK
0x04+ACK
Setup Write to [0x4C] + ACK
0x03+ACK
0x04+ACK

I want to know Under what circumstances will TMP451 detect OPEN Fault? Will TMP451 fail if an abnormal register is written? (e.g., write to register 0x03 above)

Could you help to answer the above questions? Thank you

  • Hello Xiaochen,

    The open fault condition implies that TMP451 does not detect a remote junction. The detection circuitry consists of a voltage comparator that trips when the voltage at D+ exceeds (V+) – 0.3 V (typical). The comparator output is continuously checked during a conversion. If a fault is detected, then OPEN (bit 2) in the status register is set to 1. If an abnormal register is written, then a setting would change within the temperature sensors either enabling the alert, going into shutdown mode, changing the alert functionality to THERM, or changing the temperature reading range. To help further this issue can you send an oscilloscope capture the D+ signal under the condition that it generated alert?

    Best Regards,

    Meredith McKean

  • Hi Meredith,

    We do not have the waveforms at the fault site yet . The waveform during normal operation can be attached, and we ensure that the signal of D+ is acceptable and within the design range.

  • Hello Xiaochen,

    The signal that you provided looks like it would function but it is a little noisy. Is this the signal right after power up or after restart? Can you provide the signal right after power up?

    Best Regards,

    Meredith McKean

  • Hi Meredith,

    we physically disconnected the resistor between SOC and tmp451-Q1, the 0x02 register comes 0x0C, (open and Rlow), but actually the issue we met the 0x02 register comes 0x84( only open fault), So I think it not a physical bug as it recovered in next power cycle, right? so M y question is that what will cause the tmp451-Q1 get ge OPEN fault?  thanks.

  • Hi Meredith,

    The signal provided is the signal just after the power on. The green one is the power supply of the TMP451, and the yellow one is the D+ input signal of the TMP451.

  • Hello Xiaochen,

    An open fault implies that there is a disconnection between the remote junction and TMP451. There could be a issue with power sequencing. Is the BJT embedded into an IC? Assuming its embedded, is the power stable to the embedded junction ESD structures? It is likely confused by the junction behavior at power on.

    Best Regards,

    Meredith McKean

  • hi TI expert, we catch the failed waveform as below, when we write register 0x09 to 0x40 ,which means let tmp451 enter SDmode, and the alert pin of tmp451 drive low and report OPEN fail. and the yellow channel is D+ , I think there is no obvious  abnormal. could you help to explain why entering SD mode and report OPEN ocassionally.thanks,

  • Hello Ziyang,

    There should not be a connection between SD mode and the alert line pulling low. An open condition is when the D+ exceeds (V+) – 0.3 V. The D+ may be idle between conversions. A short condition is when D+ is 0V. What was in the configuration register before writing 0x40? Can you provide a register dump before and after this change? What are your alert and therm limits set to? What are your status bits?

    Best Regards,

    Meredith McKean

  • hi TI expert

    What was in the configuration register before writing 0x40?

    A:0x00

    add aonther re-produce waveform,only a samall glitch when alert pin of tmp451 drive to LOW.  and the register dump is shown as below.

  • add normal waveform which alert pin of TMP451 stay high after writing 0x09 register to 0x40

  • Hello Ziyang,

    It sounds like the device was with default values and your wrote 0x40 to place the device in shutdown mode. I'm still confused to what you are writing to the device before the 0x40 command to the 0x09 register. The glitch makes me think that there is something else in your system causing the open status issue. Does the device recover with no additional changes or writes? 

    Best Regards,

    Meredith McKean

  • hi TI expert

    1、no writing process to tmp451 before 0x40 commands to the 0x09 register. we only read the register as below picture green  area show

    2、the glitch is so small that could not cause "OPEN " which should meet with D+ exceed V+ -0.3v, right? maybe it is caused by something wrong inside the tmp451.what I mean is that the glitch maybe a phenomenon/outcome of the "OPEN " issue;

    3、yes, the device recover (what it mean the alert pin drive high) after reading the 0x02 register (0x84) of tmp451

  • Hello Ziyang,

    This is not normal behavior for TMP451. I believe that something else is causing this issue. Is the remote junction inside another IC? If so, what IC. What are you measuring temperature of?

    Best Regards,

    Meredith McKean

  • yes, the remote junction inside another soc chip. ambient temperature 85C and water coolling 60C. the issue only happen in these condition. 

    firstly, D+ exceed V+ -0.3v, report "OPEN",exactly there is no such waveform. 

    secondly, if there is something wrong inside the SOC, what happen will cause "OPEN", the BJT inside the SOC short or open or any other issue?

  • Hello Ziyang,

    I'm currently not seeing any issues presented in this thread. I want to investigate in how the SOC device is being powered on in comparison to the local TMP451 die. Is the supply stable? If not, are there glitches? Does the SOC and TMP461 turn on at the same time? 

    Best Regards,

    Meredith McKean

  • sure , firstly tmp451 powerup , then SOC powerup and then I2C access the tmp451 and begin to configure the 0x09 register to 0x40 command.

  • and I found there is also other customers meet same issue, but also do not have RC:TMP451-Q1: TMP451 random OPEN false fault after device initialization - Sensors forum - Sensors - TI E2E support forums, Ithink it maybe something wrong with tmp451?

  • Hi Ziyang,

    The diode can sometimes be hidden when the SOC is turned off. Can you confirm through waveforms that the power lines are stable for both the SOC and TMP451?

    Best Regards,

    Meredith McKean

  • Hi Ziyang,

    The diode can sometimes be hidden when the SOC is turned off. Can you confirm through waveforms that the power lines are stable for both the SOC and TMP451?

    Best Regards,

    Meredith McKean

  • sure we can test, but if stable,then ? 

  • even it is unstable, can we see D+ exceed V+ -0.3V? is there any possible reasons that make tmp451 report "OPEN" except the D+ -0.3V?  you mean the supply for tmp451 will unstable to 0 V? 

  • Hello Ziyang,

    Lets confirm it the signal is unstable. Can you provide a schematic? I want to see what bypass caps and resistances that you are using. 

    Best Regards,

    Meredith McKean

  • Hello Ziyang,

    Thank you for providing this information. I currently do not see any issues with this thread. I want to connect you to our FAE through email. I want to look into and see if you have damaged the TMP451 is any way. I'm taking this email thread to email.

    Best Regards,

    Meredith McKean