This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: DCA1000 Questions (Ethernet Port)

Part Number: DCA1000EVM


Tool/software:

Question that i never seen answered..

I am not having success using the DCA1000 using the Mmwave introductory tutorial..

It is failing to the FPGA version..

I am unable to flash the DCA1000 FPGA 

I get

ERROR - Programming failed.

Device#1 LFE5UM-85F: Failed to verify the ID

(Expected: 0x01113043 Read: 0xFFFFFFFF).

But one question i can't get an answer for:

Should the Ethernet port light up when connect on the DCA1000?

I have connected the ethernet port from my PC (i have tried 3 PCs) using the standard ethernet cable provided and i get no lights on the ethernet port on the DCA1000 nor on my PCs

Should the ethernet port light up once you plug in the ethernet cable?

Is there anyway to verify the ethernet port is working outside of just trying the connect in the mmwave?

i get no pings from the port to the 192.168.33.30 or the FPGA ip address