Hi there,
I'm working with TMP432 temperature sensor for reading the temperature measurements within the span of -30 to +90degC for our application. I have done the implementation and able to read the temperature values from tmp432. However, I noticed that the results are not bound to within +-1 deg C accuracy as mentioned in the datasheet. Also, I observed that the temperature error is slowly increases with the ambient temperature. I attached the results for your reference. Please note that the comparision is done using precised PT100 RTD and tested in thermal chamber.
We are using 2N3906 transistor in GND collector connected mode and the auto n-factor is enabled. It will be great if you have some of the suggestions to get the accuracy right.
Regards,
Karthick