This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5013-Q1 : Recommended magnet specification

Other Parts Discussed in Thread: DRV5013-Q1

Hello,

Using DRV5013-Q1 for rotational position sensing,
is there a recommended magnet specs ?

<e.g.>
- form/size
- direction of magnetization
- density of magnetic flux

Best regards,
Junya Kato

  • Hi Kato-san,

    Our experts have been notified and should reply soon.
  • Kato-san,

    The DRV5013-Q1 is sensitive to magnetic flux in the perpendicular direction to the package.  The device should be positioned with respect to the magnet so that flux travels through the face of the package.  The simplest way to do this is what is shown in datasheet Figure 11, where the pole is near the face of the package.

    There is flexibility in the magnet size, its material, and its distance to the sensor.  Larger magnets produce more flux density at some distance.  For the DRV5013-Q1, it's important to exceed the max-BOP and decrease below the min-BRP, as the magnet turns, to ensure the thresholds are crossed.  One method you can use to determine the real flux density present is to solder a Linear Hall in place of the DRV5013-Q1 and measure its analog output voltage change.

    Best regards,
    RE

  • RE-san

    Thank you for your answer.
    It was helpful to me.

    Best regards,
    Junya Kato