Hi All,
When measuring liquid level in a tank with non-intrussive ultrasonic sensors almost all documents say the transducer should be placed in the bottom of the tank. In some case, they slightly comment the transducer can be placed in the top and I would like to ask futher details about this.
Since the wave is reflected when there is a media boundary with enough difference of impedance (sound speed) I think there would be no problem if the signal is sent from the top. When the tank is full of liquid the TOF would be shorter than when it is empty.
Why is it recommended to place the transducer on the bottom?
I list my application requirements below so anyone can advise:
- Metal tank (stainless steel).
- Different types of liquids. If the sensor is on the bottom I would need calibration for different liquids, right? But if I place the sensor on the top I think I would not need it.
- Tank heigth: 1-1,5m. (3-5 feet)
- I am mainly interested in detecting when the tank is empty. Detecting the level is a plus.
Regards, Ramon.