This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
I'm using TDC1000 C2000 evm to find the level of fluid . my TDC readings are not changing , they are constant irrespective of water is added to the container or not . it stays around 38us . im using steminc 1khz transducer which was suggested by TI also the excitation freq is 1khz . currently i do not have access to a DSO . how can you help me out here ?
also am i doing the connections right ? Im connecting one wire to TX1 (on the evm board) other one to ground (on the evm board) as explained in the manual . The transducer is tightly coupled and its attached firmly with glue .